<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 RTOS Example for S32K3</title>
    <link>https://community.nxp.com/t5/S32K/RTOS-Example-for-S32K3/m-p/1350600#M12333</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In our project we plan to use a freeRTOS OS. Currently I have not found any examples or extensions to include the library in the S32DS. Is it not released yet or it has to be done manually?&lt;/P&gt;&lt;P&gt;I found a touturial for an older version of S32DS, but it seems to be too different:&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2018/07/18/using-custom-freertos-with-s32k-and-osif-for-arm/" target="_blank"&gt;https://mcuoneclipse.com/2018/07/18/using-custom-freertos-with-s32k-and-osif-for-arm/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;And a second question about the SysTick timer. The reference manual doesn't say much about it either (how to configure or trigger an interrupt).&lt;/P&gt;&lt;P&gt;I saw that the SysTick timer is used in the OSif for the system timer. Can this timer perhaps also be used to generate a tick every 1Ms for example?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 05 Oct 2021 12:27:31 GMT</pubDate>
    <dc:creator>JoDo</dc:creator>
    <dc:date>2021-10-05T12:27:31Z</dc:date>
    <item>
      <title>RTOS Example for S32K3</title>
      <link>https://community.nxp.com/t5/S32K/RTOS-Example-for-S32K3/m-p/1350600#M12333</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In our project we plan to use a freeRTOS OS. Currently I have not found any examples or extensions to include the library in the S32DS. Is it not released yet or it has to be done manually?&lt;/P&gt;&lt;P&gt;I found a touturial for an older version of S32DS, but it seems to be too different:&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2018/07/18/using-custom-freertos-with-s32k-and-osif-for-arm/" target="_blank"&gt;https://mcuoneclipse.com/2018/07/18/using-custom-freertos-with-s32k-and-osif-for-arm/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;And a second question about the SysTick timer. The reference manual doesn't say much about it either (how to configure or trigger an interrupt).&lt;/P&gt;&lt;P&gt;I saw that the SysTick timer is used in the OSif for the system timer. Can this timer perhaps also be used to generate a tick every 1Ms for example?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Oct 2021 12:27:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RTOS-Example-for-S32K3/m-p/1350600#M12333</guid>
      <dc:creator>JoDo</dc:creator>
      <dc:date>2021-10-05T12:27:31Z</dc:date>
    </item>
  </channel>
</rss>