<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: LPSPI Debugging S32K344</title>
    <link>https://community.nxp.com/t5/S32K/LPSPI-Debugging-S32K344/m-p/1349199#M12288</link>
    <description>&lt;P&gt;Hello Daniel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much for the quick reply. That was really very helpful.&lt;/P&gt;&lt;P&gt;I guess there is no other way to watch the registers without interfere with them?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Johannes&lt;/P&gt;</description>
    <pubDate>Thu, 30 Sep 2021 14:53:11 GMT</pubDate>
    <dc:creator>JoDo</dc:creator>
    <dc:date>2021-09-30T14:53:11Z</dc:date>
    <item>
      <title>LPSPI Debugging S32K344</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-Debugging-S32K344/m-p/1349116#M12283</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I wrote a small master salve code and tried to verify the function by debugging it.&lt;/P&gt;&lt;P&gt;When I step through the code, it seems that the flags and data registers are reset by themselves (see image below). But when I run the complete code (without stepping) everything is fine. The master is transmitting and the slave is receiving correctly.&lt;/P&gt;&lt;P&gt;I am using the onboard debuger P&amp;amp;E USB MULTILINK and I have also enabled debug in the CR.&lt;/P&gt;&lt;P&gt;Does anyone have an idea what the problem is?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JoDo_0-1633002920285.png" style="width: 717px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/157996i78B994E45C6999DF/image-dimensions/717x421?v=v2" width="717" height="421" role="button" title="JoDo_0-1633002920285.png" alt="JoDo_0-1633002920285.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JoDo_0-1633002920285.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 30 Sep 2021 12:07:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-Debugging-S32K344/m-p/1349116#M12283</guid>
      <dc:creator>JoDo</dc:creator>
      <dc:date>2021-09-30T12:07:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPSPI Debugging S32K344</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-Debugging-S32K344/m-p/1349130#M12284</link>
      <description>&lt;P&gt;Hello Johannes,&lt;/P&gt;
&lt;P&gt;The RDF flag indicates the state of the RX FIFO.&lt;/P&gt;
&lt;P&gt;And the data can be read by any master from the FIFO, not only the CPU and DMA but the debugger too.&lt;/P&gt;
&lt;P&gt;You would need to close the register view and the memory view so that the Receive Data Register (RDR) is not read by the debugger.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 30 Sep 2021 12:34:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-Debugging-S32K344/m-p/1349130#M12284</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-09-30T12:34:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPSPI Debugging S32K344</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-Debugging-S32K344/m-p/1349199#M12288</link>
      <description>&lt;P&gt;Hello Daniel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much for the quick reply. That was really very helpful.&lt;/P&gt;&lt;P&gt;I guess there is no other way to watch the registers without interfere with them?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Johannes&lt;/P&gt;</description>
      <pubDate>Thu, 30 Sep 2021 14:53:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-Debugging-S32K344/m-p/1349199#M12288</guid>
      <dc:creator>JoDo</dc:creator>
      <dc:date>2021-09-30T14:53:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPSPI Debugging S32K344</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-Debugging-S32K344/m-p/1349476#M12297</link>
      <description>&lt;P&gt;Hello Johannes,&lt;/P&gt;
&lt;P&gt;Unfortunately, if the debugger reads the RDR register it is as if the CPU read it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Oct 2021 08:21:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-Debugging-S32K344/m-p/1349476#M12297</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-10-01T08:21:19Z</dc:date>
    </item>
  </channel>
</rss>