<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Triggering ADC by softeare</title>
    <link>https://community.nxp.com/t5/S32K/Triggering-ADC-by-softeare/m-p/1348981#M12277</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;if software-triggered operation is selected, a conversion is initiated&amp;nbsp;following a write to SC1A register (also defined as SC1[0], 0 is channel index)&lt;/P&gt;
&lt;P&gt;And description of ADC_DRV_ConfigChan function says...&lt;/P&gt;
&lt;P&gt;...Configures the selected control channel with the given configuration structure.&lt;/P&gt;
&lt;P&gt;When Software Trigger mode is enabled, configuring control channel index 0, implicitly triggers a new conversion on the selected ADC input channel. Therefore, ADC_DRV_ConfigChan can be used for sw-triggering conversions...&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Thu, 30 Sep 2021 07:30:52 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2021-09-30T07:30:52Z</dc:date>
    <item>
      <title>Triggering ADC by softeare</title>
      <link>https://community.nxp.com/t5/S32K/Triggering-ADC-by-softeare/m-p/1348788#M12272</link>
      <description>&lt;P&gt;HI NXP,&lt;/P&gt;&lt;P&gt;Im learning how to trigger a ADC by software, so Im working on a demo adc_swtrigger_s32k144.&lt;/P&gt;&lt;P&gt;Im confused about this API "ADC_DRV_ConfigChan(ADC_INSTANCE, 0U, &amp;amp;adConv1_ChnConfig0)".&lt;/P&gt;&lt;P&gt;Im&amp;nbsp;assuming that the "0U" here is supposed to be the 0 channel, like ADC0_SE0, but&amp;nbsp;as a matter of fact, the ADC0_SE0 is not the working channel. The real working channel is ADC0_SE12, which is PTC14, just like the demo description says.&lt;/P&gt;&lt;P&gt;So whats the meaning of "0U" here?&lt;/P&gt;</description>
      <pubDate>Thu, 30 Sep 2021 01:14:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Triggering-ADC-by-softeare/m-p/1348788#M12272</guid>
      <dc:creator>jaylou</dc:creator>
      <dc:date>2021-09-30T01:14:35Z</dc:date>
    </item>
    <item>
      <title>Re: Triggering ADC by softeare</title>
      <link>https://community.nxp.com/t5/S32K/Triggering-ADC-by-softeare/m-p/1348981#M12277</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;if software-triggered operation is selected, a conversion is initiated&amp;nbsp;following a write to SC1A register (also defined as SC1[0], 0 is channel index)&lt;/P&gt;
&lt;P&gt;And description of ADC_DRV_ConfigChan function says...&lt;/P&gt;
&lt;P&gt;...Configures the selected control channel with the given configuration structure.&lt;/P&gt;
&lt;P&gt;When Software Trigger mode is enabled, configuring control channel index 0, implicitly triggers a new conversion on the selected ADC input channel. Therefore, ADC_DRV_ConfigChan can be used for sw-triggering conversions...&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 30 Sep 2021 07:30:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Triggering-ADC-by-softeare/m-p/1348981#M12277</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-09-30T07:30:52Z</dc:date>
    </item>
  </channel>
</rss>