<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックHow to connect two phy modules through tcp/ip</title>
    <link>https://community.nxp.com/t5/S32K/How-to-connect-two-phy-modules-through-tcp-ip/m-p/1348520#M12268</link>
    <description>&lt;P&gt;Hi NXP&lt;/P&gt;&lt;P&gt;&amp;nbsp; I have two pair S32K148 evb and OM14500 PHY &lt;SPAN&gt;daughter&amp;nbsp;&lt;/SPAN&gt;boards. I want to test ethernet communication (e.g tcpip or mac &lt;SPAN&gt;broadcasting&amp;nbsp;&lt;/SPAN&gt;)with these devices, but there is no suitable demo in the examples., may I ask is there a example that can be used ?&lt;/P&gt;</description>
    <pubDate>Wed, 29 Sep 2021 16:34:08 GMT</pubDate>
    <dc:creator>sunjin</dc:creator>
    <dc:date>2021-09-29T16:34:08Z</dc:date>
    <item>
      <title>How to connect two phy modules through tcp/ip</title>
      <link>https://community.nxp.com/t5/S32K/How-to-connect-two-phy-modules-through-tcp-ip/m-p/1348520#M12268</link>
      <description>&lt;P&gt;Hi NXP&lt;/P&gt;&lt;P&gt;&amp;nbsp; I have two pair S32K148 evb and OM14500 PHY &lt;SPAN&gt;daughter&amp;nbsp;&lt;/SPAN&gt;boards. I want to test ethernet communication (e.g tcpip or mac &lt;SPAN&gt;broadcasting&amp;nbsp;&lt;/SPAN&gt;)with these devices, but there is no suitable demo in the examples., may I ask is there a example that can be used ?&lt;/P&gt;</description>
      <pubDate>Wed, 29 Sep 2021 16:34:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-connect-two-phy-modules-through-tcp-ip/m-p/1348520#M12268</guid>
      <dc:creator>sunjin</dc:creator>
      <dc:date>2021-09-29T16:34:08Z</dc:date>
    </item>
    <item>
      <title>Re: How to connect two phy modules through tcp/ip</title>
      <link>https://community.nxp.com/t5/S32K/How-to-connect-two-phy-modules-through-tcp-ip/m-p/1349483#M12298</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I checked what we have but it looks like the examples in SDK are currently all what we can provide.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 01 Oct 2021 08:34:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-connect-two-phy-modules-through-tcp-ip/m-p/1349483#M12298</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-10-01T08:34:43Z</dc:date>
    </item>
  </channel>
</rss>