<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: About Memory view windows</title>
    <link>https://community.nxp.com/t5/S32K/About-Memory-view-windows/m-p/1342694#M12158</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If a debugger shows somehting like ‚??‘ or ‚XX‘, it means that the memory access was terminated by bus error. In case of flash memory, it is a result of double bit ECC error. &lt;BR /&gt;Generally, there are three common reasons for ECC error:&lt;BR /&gt;- erase or program operation is terminated by unexpected reset, so the flash is left in undetermined state&lt;BR /&gt;- due to over-programming when we program double word which is not fully erased&lt;BR /&gt;- due to flash wear-out when too many erase-program cycles have been performed or when data retention period was exceeded&lt;BR /&gt;If you can see the question marks everywhere, it’s caused by interrupted erase operation, most likely. The solution is to erase the flash again.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Mon, 20 Sep 2021 10:32:26 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2021-09-20T10:32:26Z</dc:date>
    <item>
      <title>About Memory view windows</title>
      <link>https://community.nxp.com/t5/S32K/About-Memory-view-windows/m-p/1342487#M12147</link>
      <description>&lt;P&gt;I am learning Flash by demo flash_partitioning_s32k148, but why do my memory view windows keep showing question marks no matter which memory region I chose?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jaylou_0-1631942327840.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/156469iB5D0857C3F857039/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jaylou_0-1631942327840.png" alt="jaylou_0-1631942327840.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jaylou_0-1631942327840.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 18 Sep 2021 05:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-Memory-view-windows/m-p/1342487#M12147</guid>
      <dc:creator>jaylou</dc:creator>
      <dc:date>2021-09-18T05:18:56Z</dc:date>
    </item>
    <item>
      <title>Re: About Memory view windows</title>
      <link>https://community.nxp.com/t5/S32K/About-Memory-view-windows/m-p/1342694#M12158</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If a debugger shows somehting like ‚??‘ or ‚XX‘, it means that the memory access was terminated by bus error. In case of flash memory, it is a result of double bit ECC error. &lt;BR /&gt;Generally, there are three common reasons for ECC error:&lt;BR /&gt;- erase or program operation is terminated by unexpected reset, so the flash is left in undetermined state&lt;BR /&gt;- due to over-programming when we program double word which is not fully erased&lt;BR /&gt;- due to flash wear-out when too many erase-program cycles have been performed or when data retention period was exceeded&lt;BR /&gt;If you can see the question marks everywhere, it’s caused by interrupted erase operation, most likely. The solution is to erase the flash again.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 20 Sep 2021 10:32:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-Memory-view-windows/m-p/1342694#M12158</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-09-20T10:32:26Z</dc:date>
    </item>
  </channel>
</rss>