<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックSPI Max Length for S32k148</title>
    <link>https://community.nxp.com/t5/S32K/SPI-Max-Length-for-S32k148/m-p/1339711#M12092</link>
    <description>&lt;P&gt;Hello Community,&lt;BR /&gt;&lt;BR /&gt;I want to interface the GPU with NXP S32k148 Board via SPI for my application, so I am having Que like how much max distance i.e Cable length it will cover with max speed? with NXPs LPSPI component if I configured.&lt;BR /&gt;&lt;BR /&gt;Thanks in advance,&lt;BR /&gt;Rohit&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 14 Sep 2021 09:22:08 GMT</pubDate>
    <dc:creator>rohit_alate</dc:creator>
    <dc:date>2021-09-14T09:22:08Z</dc:date>
    <item>
      <title>SPI Max Length for S32k148</title>
      <link>https://community.nxp.com/t5/S32K/SPI-Max-Length-for-S32k148/m-p/1339711#M12092</link>
      <description>&lt;P&gt;Hello Community,&lt;BR /&gt;&lt;BR /&gt;I want to interface the GPU with NXP S32k148 Board via SPI for my application, so I am having Que like how much max distance i.e Cable length it will cover with max speed? with NXPs LPSPI component if I configured.&lt;BR /&gt;&lt;BR /&gt;Thanks in advance,&lt;BR /&gt;Rohit&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Sep 2021 09:22:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPI-Max-Length-for-S32k148/m-p/1339711#M12092</guid>
      <dc:creator>rohit_alate</dc:creator>
      <dc:date>2021-09-14T09:22:08Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Max Length for S32k148</title>
      <link>https://community.nxp.com/t5/S32K/SPI-Max-Length-for-S32k148/m-p/1339790#M12093</link>
      <description>&lt;P&gt;Hello Rohit,&lt;/P&gt;
&lt;P&gt;The LPSPI module is specified at the below conditions, so the max. load on the line is 50pF.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1631622272951.png" style="width: 655px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/156004i78D20BD3F150CA44/image-dimensions/655x172?v=v2" width="655" height="172" role="button" title="danielmartynek_0-1631622272951.png" alt="danielmartynek_0-1631622272951.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1631622272951.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 14 Sep 2021 12:26:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPI-Max-Length-for-S32k148/m-p/1339790#M12093</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-09-14T12:26:06Z</dc:date>
    </item>
  </channel>
</rss>