<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: s32k144 FTM_SignalMeasurement_Example can not work</title>
    <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/691251#M1205</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;same as this thread &lt;A href="https://community.nxp.com/thread/455092"&gt;https://community.nxp.com/thread/455092&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See discussion there...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Jul 2017 08:30:52 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2017-07-12T08:30:52Z</dc:date>
    <item>
      <title>s32k144 FTM_SignalMeasurement_Example can not work</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/691250#M1204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25680iC414DA047EEB48DC/image-size/large?v=v2&amp;amp;px=999" title="QQ截图20170711165122.png" alt="QQ截图20170711165122.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;i use the example to&amp;nbsp; test but can not work ，i did not connect error the line ，two line is pTC0 and PTB2，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when I test I find it could not into the interrupt，I change the PORT of the INPUT ，it can not work&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it have PWM out ，but the input part can not work，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what is the problem， i am crazy，could you help me&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 08:56:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/691250#M1204</guid>
      <dc:creator>jiangbolwj</dc:creator>
      <dc:date>2017-07-11T08:56:26Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 FTM_SignalMeasurement_Example can not work</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/691251#M1205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;same as this thread &lt;A href="https://community.nxp.com/thread/455092"&gt;https://community.nxp.com/thread/455092&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See discussion there...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2017 08:30:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/691251#M1205</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-07-12T08:30:52Z</dc:date>
    </item>
  </channel>
</rss>