<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Circular buffer using MBDT</title>
    <link>https://community.nxp.com/t5/S32K/Circular-buffer-using-MBDT/m-p/1335752#M11996</link>
    <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;My application needs to write to EEPROM every 1s, and as to not wear the internal EEPROM from the S32K144, I would need to implement a circular buffer. Since there are no "Circular buffer" MBDT blocks, do I need to write custom C code to access specific registers?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Rolando&lt;/P&gt;</description>
    <pubDate>Tue, 07 Sep 2021 03:01:40 GMT</pubDate>
    <dc:creator>rolo90</dc:creator>
    <dc:date>2021-09-07T03:01:40Z</dc:date>
    <item>
      <title>Circular buffer using MBDT</title>
      <link>https://community.nxp.com/t5/S32K/Circular-buffer-using-MBDT/m-p/1335752#M11996</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;My application needs to write to EEPROM every 1s, and as to not wear the internal EEPROM from the S32K144, I would need to implement a circular buffer. Since there are no "Circular buffer" MBDT blocks, do I need to write custom C code to access specific registers?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Rolando&lt;/P&gt;</description>
      <pubDate>Tue, 07 Sep 2021 03:01:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Circular-buffer-using-MBDT/m-p/1335752#M11996</guid>
      <dc:creator>rolo90</dc:creator>
      <dc:date>2021-09-07T03:01:40Z</dc:date>
    </item>
    <item>
      <title>Re: Circular buffer using MBDT</title>
      <link>https://community.nxp.com/t5/S32K/Circular-buffer-using-MBDT/m-p/1335981#M12000</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Rolando,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;For MBDT support, we have currently only the &lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt" target="_self"&gt;MBDT community&lt;/A&gt;.&lt;BR /&gt;Can you please post this issue there?&lt;BR /&gt;The community is monitored by our MBDT team.&lt;BR /&gt;Thank you for your understanding.&lt;/P&gt;
&lt;P&gt;Since I am not familiar with MBDT, I don’t know if MBDT can’t achieve this function.&lt;BR /&gt;About how to use the EEPROM, please refer: &lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN11983.pdf" target="_self"&gt;AN11983 Using the S32K1xx EEPROM Functionality&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 07 Sep 2021 08:48:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Circular-buffer-using-MBDT/m-p/1335981#M12000</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-09-07T08:48:49Z</dc:date>
    </item>
  </channel>
</rss>