<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックCLKOUT maximum frequency</title>
    <link>https://community.nxp.com/t5/S32K/CLKOUT-maximum-frequency/m-p/1334056#M11950</link>
    <description>&lt;P&gt;Hi gents,&lt;/P&gt;&lt;P&gt;S32K-DS rev.13 - par. 6.5.7 says that maximum supported clock out frequency is 20 MHz. Is this referred to all CLKOUT pins? Is it really true? Which is the reason of this limitation?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Specifically, for a S32K148 device in QFP100 powered at 3.3V, why should not be possible to output a 25 MHz signal from a FAST GPIO pin like PTD10 (pin 36)? IMHO the scenario would be the same of other FAST GPIO pins like PTC2/PTD7/PTD12 in RMII mode or PTD11 in MII mode.&lt;/P&gt;&lt;P&gt;Please also note that "S32K1xx_Clock_Calculator_Rev1" does not throw an error when CLKOUT is configured for frequencies greater than 20 MHz.&lt;/P&gt;&lt;P&gt;Thanks to all&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 02 Sep 2021 10:26:42 GMT</pubDate>
    <dc:creator>marcoelia</dc:creator>
    <dc:date>2021-09-02T10:26:42Z</dc:date>
    <item>
      <title>CLKOUT maximum frequency</title>
      <link>https://community.nxp.com/t5/S32K/CLKOUT-maximum-frequency/m-p/1334056#M11950</link>
      <description>&lt;P&gt;Hi gents,&lt;/P&gt;&lt;P&gt;S32K-DS rev.13 - par. 6.5.7 says that maximum supported clock out frequency is 20 MHz. Is this referred to all CLKOUT pins? Is it really true? Which is the reason of this limitation?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Specifically, for a S32K148 device in QFP100 powered at 3.3V, why should not be possible to output a 25 MHz signal from a FAST GPIO pin like PTD10 (pin 36)? IMHO the scenario would be the same of other FAST GPIO pins like PTC2/PTD7/PTD12 in RMII mode or PTD11 in MII mode.&lt;/P&gt;&lt;P&gt;Please also note that "S32K1xx_Clock_Calculator_Rev1" does not throw an error when CLKOUT is configured for frequencies greater than 20 MHz.&lt;/P&gt;&lt;P&gt;Thanks to all&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Sep 2021 10:26:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CLKOUT-maximum-frequency/m-p/1334056#M11950</guid>
      <dc:creator>marcoelia</dc:creator>
      <dc:date>2021-09-02T10:26:42Z</dc:date>
    </item>
    <item>
      <title>Re: CLKOUT maximum frequency</title>
      <link>https://community.nxp.com/t5/S32K/CLKOUT-maximum-frequency/m-p/1336361#M12009</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Marco,&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Robin_Shen_0-1631062498185.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/155392iD2B49F5D928F7F83/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Robin_Shen_0-1631062498185.png" alt="Robin_Shen_0-1631062498185.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I use &lt;STRONG&gt;CLKOUTSEL&lt;/STRONG&gt; to select a frequency higher than 20MHz through the &lt;STRONG&gt;CLKOUT&lt;/STRONG&gt; pin, and I can observe the waveform on the oscilloscope.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regarding your proposed plan, use CLKOUT to feed the 25 MHz clock input of their on-board Ethernet PHY (&lt;A href="http://ww1.microchip.com/downloads/en/devicedoc/00002199a.pdf" target="_blank" rel="noopener nofollow noreferrer"&gt;KSZ8081RNA&lt;/A&gt;, pin 8).&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;After discussed with hardware team, we think it's possible to use in such case. But please remind:&lt;BR /&gt;1. select a fast type pad GPIO pin for CLKOUT;&lt;BR /&gt;2. configure corresponding&amp;nbsp;PCR[&lt;STRONG&gt;DSE&lt;/STRONG&gt;] =&amp;nbsp;1&amp;nbsp;to ensure its output strength;&lt;BR /&gt;3. recommend to add a clock buffer if BOM cost allowed.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 01:03:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CLKOUT-maximum-frequency/m-p/1336361#M12009</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-09-08T01:03:54Z</dc:date>
    </item>
  </channel>
</rss>