<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic demo code for flash_partitioning_s32k148 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/demo-code-for-flash-partitioning-s32k148/m-p/1333798#M11931</link>
    <description>&lt;P&gt;FTFx_FCCOB0 = FTFx_ERASE_SECTOR;&lt;BR /&gt;FTFx_FCCOB1 = GET_BIT_16_23(dest);&lt;BR /&gt;FTFx_FCCOB2 = GET_BIT_8_15(dest);&lt;BR /&gt;FTFx_FCCOB3 = GET_BIT_0_7(dest);&lt;/P&gt;&lt;P&gt;this is the&amp;nbsp;Passing parameter command, but what is the exactly address?&lt;/P&gt;</description>
    <pubDate>Thu, 02 Sep 2021 04:59:08 GMT</pubDate>
    <dc:creator>jaylou</dc:creator>
    <dc:date>2021-09-02T04:59:08Z</dc:date>
    <item>
      <title>demo code for flash_partitioning_s32k148</title>
      <link>https://community.nxp.com/t5/S32K/demo-code-for-flash-partitioning-s32k148/m-p/1333798#M11931</link>
      <description>&lt;P&gt;FTFx_FCCOB0 = FTFx_ERASE_SECTOR;&lt;BR /&gt;FTFx_FCCOB1 = GET_BIT_16_23(dest);&lt;BR /&gt;FTFx_FCCOB2 = GET_BIT_8_15(dest);&lt;BR /&gt;FTFx_FCCOB3 = GET_BIT_0_7(dest);&lt;/P&gt;&lt;P&gt;this is the&amp;nbsp;Passing parameter command, but what is the exactly address?&lt;/P&gt;</description>
      <pubDate>Thu, 02 Sep 2021 04:59:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/demo-code-for-flash-partitioning-s32k148/m-p/1333798#M11931</guid>
      <dc:creator>jaylou</dc:creator>
      <dc:date>2021-09-02T04:59:08Z</dc:date>
    </item>
    <item>
      <title>Re: demo code for flash_partitioning_s32k148</title>
      <link>https://community.nxp.com/t5/S32K/demo-code-for-flash-partitioning-s32k148/m-p/1333926#M11938</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;FCCOBn registers are 8bit registers, so the address is split to FCCOB1-3. The address is 24bit only which is sufficient to cover whole flash.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 02 Sep 2021 07:33:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/demo-code-for-flash-partitioning-s32k148/m-p/1333926#M11938</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-09-02T07:33:33Z</dc:date>
    </item>
    <item>
      <title>Re: demo code for flash_partitioning_s32k148</title>
      <link>https://community.nxp.com/t5/S32K/demo-code-for-flash-partitioning-s32k148/m-p/1338749#M12066</link>
      <description>&lt;P&gt;Thank you, Sir.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Sep 2021 03:07:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/demo-code-for-flash-partitioning-s32k148/m-p/1338749#M12066</guid>
      <dc:creator>jaylou</dc:creator>
      <dc:date>2021-09-13T03:07:26Z</dc:date>
    </item>
  </channel>
</rss>