<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32k flexIO shifter match store mode</title>
    <link>https://community.nxp.com/t5/S32K/S32k-flexIO-shifter-match-store-mode/m-p/1332696#M11904</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; in match store mode,&amp;nbsp; the manual says higher 16 bits are used to set the data to be matched and the lower to mask the results.&amp;nbsp; Since the shifter is 32bit, so how does it be compared to SHIFTBUF[31:16], and how data is received when a match occurs?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 31 Aug 2021 20:44:08 GMT</pubDate>
    <dc:creator>yuegao1996</dc:creator>
    <dc:date>2021-08-31T20:44:08Z</dc:date>
    <item>
      <title>S32k flexIO shifter match store mode</title>
      <link>https://community.nxp.com/t5/S32K/S32k-flexIO-shifter-match-store-mode/m-p/1332696#M11904</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; in match store mode,&amp;nbsp; the manual says higher 16 bits are used to set the data to be matched and the lower to mask the results.&amp;nbsp; Since the shifter is 32bit, so how does it be compared to SHIFTBUF[31:16], and how data is received when a match occurs?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 31 Aug 2021 20:44:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k-flexIO-shifter-match-store-mode/m-p/1332696#M11904</guid>
      <dc:creator>yuegao1996</dc:creator>
      <dc:date>2021-08-31T20:44:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32k flexIO shifter match store mode</title>
      <link>https://community.nxp.com/t5/S32K/S32k-flexIO-shifter-match-store-mode/m-p/1332814#M11911</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;yuegao1996&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; You can refer to the process in the figure below.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1630464166985.png" style="width: 554px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/154723i15F45F5A10262E10/image-dimensions/554x438?v=v2" width="554" height="438" role="button" title="Senlent_0-1630464166985.png" alt="Senlent_0-1630464166985.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR!&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Jim,&lt;/P&gt;</description>
      <pubDate>Wed, 01 Sep 2021 02:51:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k-flexIO-shifter-match-store-mode/m-p/1332814#M11911</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2021-09-01T02:51:21Z</dc:date>
    </item>
    <item>
      <title>Re: S32k flexIO shifter match store mode</title>
      <link>https://community.nxp.com/t5/S32K/S32k-flexIO-shifter-match-store-mode/m-p/1332893#M11914</link>
      <description>&lt;P&gt;Hi Jim,&amp;nbsp;&lt;/P&gt;&lt;P&gt;does this mean that as far as the higher 16 bits matched, then the whole 32 bit data in the shifter will be loaded to the shiftbuf?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;many thanks,&lt;/P&gt;&lt;P&gt;Yuri&lt;/P&gt;</description>
      <pubDate>Wed, 01 Sep 2021 05:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k-flexIO-shifter-match-store-mode/m-p/1332893#M11914</guid>
      <dc:creator>yuegao1996</dc:creator>
      <dc:date>2021-09-01T05:31:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32k flexIO shifter match store mode</title>
      <link>https://community.nxp.com/t5/S32K/S32k-flexIO-shifter-match-store-mode/m-p/1332931#M11915</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;yuegao1996&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;yes, I think it should be like this.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; The step"n+2"&amp;nbsp; says: "when match occur store shifter data into the buffer, and set some flag bit".&lt;/P&gt;</description>
      <pubDate>Wed, 01 Sep 2021 06:22:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k-flexIO-shifter-match-store-mode/m-p/1332931#M11915</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2021-09-01T06:22:48Z</dc:date>
    </item>
  </channel>
</rss>