<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K STATUS UART RX OVERRUN WHILE AD WITH DMA</title>
    <link>https://community.nxp.com/t5/S32K/S32K-STATUS-UART-RX-OVERRUN-WHILE-AD-WITH-DMA/m-p/1332506#M11899</link>
    <description>&lt;P&gt;Hello Mates,&lt;/P&gt;&lt;P&gt;my S32K is using the UART as modbus 485, eventually during the AD through DMA capture (very long, 7000 captures or so) the UART gets&amp;nbsp;STATUS UART RX OVERRUN error on a interrupt..&lt;/P&gt;&lt;P&gt;I've it fixed using the deinit and restarting it, it works but I believe this is not necessary.&lt;/P&gt;&lt;P&gt;Any tips of why the DMA capture end interrupt maybe conflicting my UART interrupt? Priorities, maybe?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Greetings from Brazil, Renan&lt;/P&gt;</description>
    <pubDate>Tue, 31 Aug 2021 11:43:50 GMT</pubDate>
    <dc:creator>rvalente</dc:creator>
    <dc:date>2021-08-31T11:43:50Z</dc:date>
    <item>
      <title>S32K STATUS UART RX OVERRUN WHILE AD WITH DMA</title>
      <link>https://community.nxp.com/t5/S32K/S32K-STATUS-UART-RX-OVERRUN-WHILE-AD-WITH-DMA/m-p/1332506#M11899</link>
      <description>&lt;P&gt;Hello Mates,&lt;/P&gt;&lt;P&gt;my S32K is using the UART as modbus 485, eventually during the AD through DMA capture (very long, 7000 captures or so) the UART gets&amp;nbsp;STATUS UART RX OVERRUN error on a interrupt..&lt;/P&gt;&lt;P&gt;I've it fixed using the deinit and restarting it, it works but I believe this is not necessary.&lt;/P&gt;&lt;P&gt;Any tips of why the DMA capture end interrupt maybe conflicting my UART interrupt? Priorities, maybe?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Greetings from Brazil, Renan&lt;/P&gt;</description>
      <pubDate>Tue, 31 Aug 2021 11:43:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-STATUS-UART-RX-OVERRUN-WHILE-AD-WITH-DMA/m-p/1332506#M11899</guid>
      <dc:creator>rvalente</dc:creator>
      <dc:date>2021-08-31T11:43:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32K STATUS UART RX OVERRUN WHILE AD WITH DMA</title>
      <link>https://community.nxp.com/t5/S32K/S32K-STATUS-UART-RX-OVERRUN-WHILE-AD-WITH-DMA/m-p/1333283#M11926</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181060"&gt;@rvalente&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Yes, you can set a higher interrupt priority for the UART.&lt;/P&gt;
&lt;P&gt;Maybe you have a long DMA complete interrupt routine that can't be preempted by a lower-priority UART interrupt.&lt;/P&gt;
&lt;P&gt;Or you can just increase the system clock frequency.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 01 Sep 2021 13:41:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-STATUS-UART-RX-OVERRUN-WHILE-AD-WITH-DMA/m-p/1333283#M11926</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-09-01T13:41:19Z</dc:date>
    </item>
  </channel>
</rss>