<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: s32k144 csec : Boot Ok Command in S32K</title>
    <link>https://community.nxp.com/t5/S32K/s32k144-csec-Boot-Ok-Command/m-p/1331121#M11865</link>
    <description>&lt;P&gt;Hi Phillip,&lt;/P&gt;
&lt;P&gt;I got very fast feedback which confirmed my thoughts. CMD_BOOT_OK is not needed to use boot protected keys and it meets the SHE spec. The sentence in the app note will be updated.&lt;/P&gt;
&lt;P&gt;Thanks for pointing this out.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Fri, 27 Aug 2021 15:59:10 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2021-08-27T15:59:10Z</dc:date>
    <item>
      <title>s32k144 csec : Boot Ok Command</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-csec-Boot-Ok-Command/m-p/1330132#M11836</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have been studying 'Secure Boot' in csec.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In AN5401, Page 20&lt;/P&gt;&lt;P&gt;==========================================================================&lt;/P&gt;&lt;P&gt;If the secure boot process is successful and CMD_BOOT_OK is executed, keys marked as Boot Protected (BOOT_PROT) can&lt;BR /&gt;be used by the application code. Otherwise boot protected keys remain locked for application use.&lt;/P&gt;&lt;P&gt;==========================================================================&lt;/P&gt;&lt;P&gt;So my application is checking the secure boot status through "FTFC-&amp;gt;FCSESTAT" .&lt;/P&gt;&lt;P&gt;and when boot mac verifying is succeeded, the application calls "CSEC_DRV_BootOK()".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And I tested boot protection flag key.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But, regardless of calling "CSEC_DRV_BootOK()", I could use the boot protection flag key,&lt;/P&gt;&lt;P&gt;As long as, the boot mac verifying is&amp;nbsp;succeeded.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do i misunderstand AN5401?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Phillip&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 07:52:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-csec-Boot-Ok-Command/m-p/1330132#M11836</guid>
      <dc:creator>kmh48301</dc:creator>
      <dc:date>2021-08-26T07:52:34Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 csec : Boot Ok Command</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-csec-Boot-Ok-Command/m-p/1330998#M11863</link>
      <description>&lt;P&gt;Hi Phillip,&lt;/P&gt;
&lt;P&gt;I can see that SHE specification does not explicitly say that CMD_BOOT_OK is needed to unprotect boot protected keys. It is used rather to lock CMD_BOOT_FAILURE command. In my opinion, the behavior you can see complies with the spec and the sentence in the AN is wrong.&lt;/P&gt;
&lt;P&gt;But let me double check this. Notice that it will probably take a couple of days.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Aug 2021 11:18:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-csec-Boot-Ok-Command/m-p/1330998#M11863</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-08-27T11:18:08Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 csec : Boot Ok Command</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-csec-Boot-Ok-Command/m-p/1331121#M11865</link>
      <description>&lt;P&gt;Hi Phillip,&lt;/P&gt;
&lt;P&gt;I got very fast feedback which confirmed my thoughts. CMD_BOOT_OK is not needed to use boot protected keys and it meets the SHE spec. The sentence in the app note will be updated.&lt;/P&gt;
&lt;P&gt;Thanks for pointing this out.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 27 Aug 2021 15:59:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-csec-Boot-Ok-Command/m-p/1331121#M11865</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-08-27T15:59:10Z</dc:date>
    </item>
  </channel>
</rss>