<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Disable Flash Command Complete interrupt in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Disable-Flash-Command-Complete-interrupt/m-p/1329020#M11809</link>
    <description>&lt;P&gt;already got the answer, its simple, LOL&lt;/P&gt;</description>
    <pubDate>Wed, 25 Aug 2021 02:51:35 GMT</pubDate>
    <dc:creator>jaylou</dc:creator>
    <dc:date>2021-08-25T02:51:35Z</dc:date>
    <item>
      <title>Disable Flash Command Complete interrupt</title>
      <link>https://community.nxp.com/t5/S32K/Disable-Flash-Command-Complete-interrupt/m-p/1328971#M11804</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm a newbie, but how do you&amp;nbsp;Disable Flash Command Complete interrupt by these lines?&lt;/P&gt;&lt;P&gt;void CCIF_Handler(void)&lt;BR /&gt;{&lt;BR /&gt;/* Disable Flash Command Complete interrupt */&lt;BR /&gt;FTFx_FCNFG &amp;amp;= (~FTFx_FCNFG_CCIE_MASK);&lt;/P&gt;&lt;P&gt;return;&lt;BR /&gt;}&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 01:26:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Disable-Flash-Command-Complete-interrupt/m-p/1328971#M11804</guid>
      <dc:creator>jaylou</dc:creator>
      <dc:date>2021-08-25T01:26:25Z</dc:date>
    </item>
    <item>
      <title>Re: Disable Flash Command Complete interrupt</title>
      <link>https://community.nxp.com/t5/S32K/Disable-Flash-Command-Complete-interrupt/m-p/1329020#M11809</link>
      <description>&lt;P&gt;already got the answer, its simple, LOL&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 02:51:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Disable-Flash-Command-Complete-interrupt/m-p/1329020#M11809</guid>
      <dc:creator>jaylou</dc:creator>
      <dc:date>2021-08-25T02:51:35Z</dc:date>
    </item>
  </channel>
</rss>