<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Program S32K142 Over CAN</title>
    <link>https://community.nxp.com/t5/S32K/Program-S32K142-Over-CAN/m-p/1321223#M11649</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to find a can bus supporting bootloader for the S32K142 (I'm currently working on the eval kit however this will soon be a custom solution). The application is automotive and the requirement is to be able to update the firmware remotely&amp;nbsp;via can once the device is fitted and not easily accessible.&lt;/P&gt;&lt;P&gt;The application code is built using the model based design toolbox and the ideal solution to update the firmware is to have a (windows) gui in which to load the .elf file and set the application code start address and code size range, then program from the PC over can. For initial bootloader programming, programming over JTAG or by using the OpenSDA is acceptable.&lt;/P&gt;&lt;P&gt;It looks like the RAppID BL Tool is the best option, however the latest version (1.6.7.35) only supports the S32K144 under the MCU drop down menu. Is there an available bootloader for the S32K142 which would enable this use case?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Jonny&lt;/P&gt;</description>
    <pubDate>Tue, 10 Aug 2021 15:53:09 GMT</pubDate>
    <dc:creator>JonnySchmidt</dc:creator>
    <dc:date>2021-08-10T15:53:09Z</dc:date>
    <item>
      <title>Program S32K142 Over CAN</title>
      <link>https://community.nxp.com/t5/S32K/Program-S32K142-Over-CAN/m-p/1321223#M11649</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to find a can bus supporting bootloader for the S32K142 (I'm currently working on the eval kit however this will soon be a custom solution). The application is automotive and the requirement is to be able to update the firmware remotely&amp;nbsp;via can once the device is fitted and not easily accessible.&lt;/P&gt;&lt;P&gt;The application code is built using the model based design toolbox and the ideal solution to update the firmware is to have a (windows) gui in which to load the .elf file and set the application code start address and code size range, then program from the PC over can. For initial bootloader programming, programming over JTAG or by using the OpenSDA is acceptable.&lt;/P&gt;&lt;P&gt;It looks like the RAppID BL Tool is the best option, however the latest version (1.6.7.35) only supports the S32K144 under the MCU drop down menu. Is there an available bootloader for the S32K142 which would enable this use case?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Jonny&lt;/P&gt;</description>
      <pubDate>Tue, 10 Aug 2021 15:53:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Program-S32K142-Over-CAN/m-p/1321223#M11649</guid>
      <dc:creator>JonnySchmidt</dc:creator>
      <dc:date>2021-08-10T15:53:09Z</dc:date>
    </item>
    <item>
      <title>Re: Program S32K142 Over CAN</title>
      <link>https://community.nxp.com/t5/S32K/Program-S32K142-Over-CAN/m-p/1321958#M11652</link>
      <description>&lt;P&gt;Hi Jonny,&lt;/P&gt;
&lt;P&gt;You can use the Unified Bootloader, it is ported to S32K142.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1628692206219.png" style="width: 600px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/152633iB3E557BBCA328F1B/image-dimensions/600x114?v=v2" width="600" height="114" role="button" title="danielmartynek_0-1628692206219.png" alt="danielmartynek_0-1628692206219.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mcus/s32k1-microcontrollers-for-general-purpose:S32K1?tab=Design_Tools_Tab" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mcus/s32k1-microcontrollers-for-general-purpose:S32K1?tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Aug 2021 14:31:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Program-S32K142-Over-CAN/m-p/1321958#M11652</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-08-11T14:31:24Z</dc:date>
    </item>
    <item>
      <title>Re: Program S32K142 Over CAN</title>
      <link>https://community.nxp.com/t5/S32K/Program-S32K142-Over-CAN/m-p/1322468#M11660</link>
      <description>&lt;P&gt;Thanks Daniel,&lt;/P&gt;&lt;P&gt;Thanks, based on other posts in the community forums, I have now also raised a support ticket (&lt;SPAN&gt;00414468&lt;/SPAN&gt;), requesting the NXP OpenBus software tool used to flash the chips as there's no download available.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Jonny&lt;/P&gt;</description>
      <pubDate>Thu, 12 Aug 2021 07:48:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Program-S32K142-Over-CAN/m-p/1322468#M11660</guid>
      <dc:creator>JonnySchmidt</dc:creator>
      <dc:date>2021-08-12T07:48:02Z</dc:date>
    </item>
    <item>
      <title>Re: Program S32K142 Over CAN</title>
      <link>https://community.nxp.com/t5/S32K/Program-S32K142-Over-CAN/m-p/1322512#M11664</link>
      <description>&lt;P&gt;I've received the tool now via support. Thanks again for your help.&lt;/P&gt;&lt;P&gt;Jonny&lt;/P&gt;</description>
      <pubDate>Thu, 12 Aug 2021 08:42:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Program-S32K142-Over-CAN/m-p/1322512#M11664</guid>
      <dc:creator>JonnySchmidt</dc:creator>
      <dc:date>2021-08-12T08:42:19Z</dc:date>
    </item>
  </channel>
</rss>