<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32_K144_bootloader Linker file</title>
    <link>https://community.nxp.com/t5/S32K/S32-K144-bootloader-Linker-file/m-p/1319200#M11562</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;S32K144_64_flash_bootloader.ld&lt;/STRONG&gt; is obviously customized linker file which is not generated by S32DS. If you are moving to another derivative, it will be necessary to manually update the linker file as needed (S32K142 has less RAM and flash). &lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Thu, 05 Aug 2021 16:34:49 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2021-08-05T16:34:49Z</dc:date>
    <item>
      <title>S32_K144_bootloader Linker file</title>
      <link>https://community.nxp.com/t5/S32K/S32-K144-bootloader-Linker-file/m-p/1317622#M11521</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I ported my application from S32k144 to S32K142_64, but the S32K144_100 Project contains&amp;nbsp;&lt;STRONG&gt;S32K144_64_flash_bootloader.ld, and I'm&amp;nbsp;&lt;/STRONG&gt;unable to generate this file for S32K142_64.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And One more issue I'm facing is that when I'm generating processor expert file I'm getting &lt;STRONG&gt;trgmux.chg undefined CPU type S32K142_64.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;All suggestions are welcome.&lt;/P&gt;&lt;P&gt;Ta&lt;/P&gt;</description>
      <pubDate>Wed, 04 Aug 2021 01:55:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32-K144-bootloader-Linker-file/m-p/1317622#M11521</guid>
      <dc:creator>arun_07</dc:creator>
      <dc:date>2021-08-04T01:55:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32_K144_bootloader Linker file</title>
      <link>https://community.nxp.com/t5/S32K/S32-K144-bootloader-Linker-file/m-p/1319200#M11562</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;S32K144_64_flash_bootloader.ld&lt;/STRONG&gt; is obviously customized linker file which is not generated by S32DS. If you are moving to another derivative, it will be necessary to manually update the linker file as needed (S32K142 has less RAM and flash). &lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 05 Aug 2021 16:34:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32-K144-bootloader-Linker-file/m-p/1319200#M11562</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-08-05T16:34:49Z</dc:date>
    </item>
  </channel>
</rss>