<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: About LPSPI circular FIFO in S32K</title>
    <link>https://community.nxp.com/t5/S32K/About-LPSPI-circular-FIFO/m-p/1317140#M11509</link>
    <description>&lt;P&gt;不客气&lt;/P&gt;</description>
    <pubDate>Tue, 03 Aug 2021 07:48:58 GMT</pubDate>
    <dc:creator>Senlent</dc:creator>
    <dc:date>2021-08-03T07:48:58Z</dc:date>
    <item>
      <title>About LPSPI circular FIFO</title>
      <link>https://community.nxp.com/t5/S32K/About-LPSPI-circular-FIFO/m-p/1316750#M11492</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;about&amp;nbsp;LPSPI circular FIFO, the RM says:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After the transmit/command FIFO is considered empty and the LPSPI is idle, the FIFO read pointer is restored with the saved version, so the contents of the transmit/command FIFO are not permanently pulled from the FIFO while circular FIFO mode is enabled.&lt;/P&gt;&lt;P&gt;does it mean the previous data in the FIFO won't be cleared and will repeatedly transfer the data ?&lt;/P&gt;&lt;P&gt;or it just transmits the data of that short addr?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks a lot,&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Yuri&lt;/P&gt;</description>
      <pubDate>Mon, 02 Aug 2021 13:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-LPSPI-circular-FIFO/m-p/1316750#M11492</guid>
      <dc:creator>yuegao1996</dc:creator>
      <dc:date>2021-08-02T13:30:57Z</dc:date>
    </item>
    <item>
      <title>Re: About LPSPI circular FIFO</title>
      <link>https://community.nxp.com/t5/S32K/About-LPSPI-circular-FIFO/m-p/1316952#M11501</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@yuegao1996" target="_blank"&gt;Hi@yuegao1996&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;我就用中文回你了，这样比较快点。数据手册中的内容翻译：&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;发送/命令FIFO还支持循环FIFO功能。 这使LPSPI主控器可以（周期性地）重复一段短的数据传输，该传输可以适合发送/命令FIFO，而无需其他FIFO访问。 启用循环FIFO后，将保存FIFO读取指针的当前状态，并且状态标志不会更新。 一旦发送/命令FIFO被认为是空的并且LPSPI处于空闲状态，则FIFO读取指针将与保存的版本一起恢复，因此当启用循环FIFO模式时，发送/命令FIFO的内容不会被永久从FIFO中拉出。&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;按我的理解就是FIFO就是一个有深度的数组了，使能循环FIFO功能以后，指向当前数组的指针不跳了（之前应该是发送一个指针值就向下跳一个地址），那你发送的一直是当前指针的值（当然我觉得也可以是之前的，因为FIFO没有清空，之前的值也应该是存在的）。所以你说FIFO的先前的值应该也是不会被清空的。&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;这个我觉得你还是写个代码验证下，光看手册总是会有点混淆，在S32 DS的IDE里面已经有配置好的例程，你可以参考或者简单修改下。我在网上随便搜索了下，有一个叫S32K-LPSIP中文手册的帖子写的挺详细，你要是在学习LPSPI的话可能对你有帮助，这里我不方便贴出具体的链接，你自己搜索吧。&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Jim.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Aug 2021 01:44:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-LPSPI-circular-FIFO/m-p/1316952#M11501</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2021-08-03T01:44:50Z</dc:date>
    </item>
    <item>
      <title>Re: About LPSPI circular FIFO</title>
      <link>https://community.nxp.com/t5/S32K/About-LPSPI-circular-FIFO/m-p/1317135#M11508</link>
      <description>&lt;P&gt;好的， 谢谢前辈！&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Yuri&lt;/P&gt;</description>
      <pubDate>Tue, 03 Aug 2021 07:46:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-LPSPI-circular-FIFO/m-p/1317135#M11508</guid>
      <dc:creator>yuegao1996</dc:creator>
      <dc:date>2021-08-03T07:46:01Z</dc:date>
    </item>
    <item>
      <title>Re: About LPSPI circular FIFO</title>
      <link>https://community.nxp.com/t5/S32K/About-LPSPI-circular-FIFO/m-p/1317140#M11509</link>
      <description>&lt;P&gt;不客气&lt;/P&gt;</description>
      <pubDate>Tue, 03 Aug 2021 07:48:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-LPSPI-circular-FIFO/m-p/1317140#M11509</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2021-08-03T07:48:58Z</dc:date>
    </item>
  </channel>
</rss>