<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックAbout the button</title>
    <link>https://community.nxp.com/t5/S32K/About-the-button/m-p/1311248#M11417</link>
    <description>&lt;P&gt;When I use a key, I assign a value to a variable using keys 1 and 2 respectively, but it's strange why I can assign a value only on the first press. I added the ability to assign a value to a variable in the key action section of the can_pal demo, in which I receive a new value every time. Why is that? It's Fang's where I use the buttons&lt;/P&gt;</description>
    <pubDate>Wed, 21 Jul 2021 10:48:18 GMT</pubDate>
    <dc:creator>kalajiao</dc:creator>
    <dc:date>2021-07-21T10:48:18Z</dc:date>
    <item>
      <title>About the button</title>
      <link>https://community.nxp.com/t5/S32K/About-the-button/m-p/1311248#M11417</link>
      <description>&lt;P&gt;When I use a key, I assign a value to a variable using keys 1 and 2 respectively, but it's strange why I can assign a value only on the first press. I added the ability to assign a value to a variable in the key action section of the can_pal demo, in which I receive a new value every time. Why is that? It's Fang's where I use the buttons&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jul 2021 10:48:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-the-button/m-p/1311248#M11417</guid>
      <dc:creator>kalajiao</dc:creator>
      <dc:date>2021-07-21T10:48:18Z</dc:date>
    </item>
    <item>
      <title>Re: About the button</title>
      <link>https://community.nxp.com/t5/S32K/About-the-button/m-p/1311784#M11423</link>
      <description>&lt;P&gt;Seems that you forget&amp;nbsp;&lt;STRONG&gt;Clear interrupt flag.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Clear interrupt flag.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/150543i72B43088F65F1F2D/image-size/large?v=v2&amp;amp;px=999" role="button" title="Clear interrupt flag.jpg" alt="Clear interrupt flag.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Clear interrupt flag.jpg&lt;/span&gt;&lt;/span&gt;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;You can set a breakpoint in the buttonisr function to check whether it will enter this function every time you press a key.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jul 2021 06:59:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-the-button/m-p/1311784#M11423</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-07-22T06:59:49Z</dc:date>
    </item>
  </channel>
</rss>