<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K148, S32DS CAN Driver Performance Issues.</title>
    <link>https://community.nxp.com/t5/S32K/S32K148-S32DS-CAN-Driver-Performance-Issues/m-p/1300140#M11225</link>
    <description>&lt;P&gt;SDK Version : 3.0.0&lt;/P&gt;&lt;P&gt;Is there any testing statistics for CAN Drivers provided in the SDK?&lt;/P&gt;&lt;P&gt;Currently I see that CAN driver keeps missing frames on the bus. This is happening with flash tool that works over UDS, and when the CAN frame distance is less than 0.6msec apart.&lt;/P&gt;&lt;P&gt;What is the recommended time distance between consecutive message?&lt;/P&gt;&lt;P&gt;CAN Configuration used is individual Mailbox based configuration.(Not FiFO)&lt;/P&gt;&lt;P&gt;Till 45% of the bus load, I do get proper communication, but after that it seems to missing messages.&lt;/P&gt;&lt;P&gt;Any pointer to resolve the same?&lt;/P&gt;</description>
    <pubDate>Wed, 30 Jun 2021 06:05:57 GMT</pubDate>
    <dc:creator>Vijay_Arwapally</dc:creator>
    <dc:date>2021-06-30T06:05:57Z</dc:date>
    <item>
      <title>S32K148, S32DS CAN Driver Performance Issues.</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-S32DS-CAN-Driver-Performance-Issues/m-p/1300140#M11225</link>
      <description>&lt;P&gt;SDK Version : 3.0.0&lt;/P&gt;&lt;P&gt;Is there any testing statistics for CAN Drivers provided in the SDK?&lt;/P&gt;&lt;P&gt;Currently I see that CAN driver keeps missing frames on the bus. This is happening with flash tool that works over UDS, and when the CAN frame distance is less than 0.6msec apart.&lt;/P&gt;&lt;P&gt;What is the recommended time distance between consecutive message?&lt;/P&gt;&lt;P&gt;CAN Configuration used is individual Mailbox based configuration.(Not FiFO)&lt;/P&gt;&lt;P&gt;Till 45% of the bus load, I do get proper communication, but after that it seems to missing messages.&lt;/P&gt;&lt;P&gt;Any pointer to resolve the same?&lt;/P&gt;</description>
      <pubDate>Wed, 30 Jun 2021 06:05:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-S32DS-CAN-Driver-Performance-Issues/m-p/1300140#M11225</guid>
      <dc:creator>Vijay_Arwapally</dc:creator>
      <dc:date>2021-06-30T06:05:57Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148, S32DS CAN Driver Performance Issues.</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-S32DS-CAN-Driver-Performance-Issues/m-p/1301511#M11246</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/61445"&gt;@nxp&lt;/a&gt;: Can someone address the query ASAP?&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jul 2021 05:18:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-S32DS-CAN-Driver-Performance-Issues/m-p/1301511#M11246</guid>
      <dc:creator>Vijay_Arwapally</dc:creator>
      <dc:date>2021-07-02T05:18:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148, S32DS CAN Driver Performance Issues.</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-S32DS-CAN-Driver-Performance-Issues/m-p/1302256#M11262</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/61445"&gt;@nxp&lt;/a&gt;Repond!&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jul 2021 06:44:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-S32DS-CAN-Driver-Performance-Issues/m-p/1302256#M11262</guid>
      <dc:creator>Vijay_Arwapally</dc:creator>
      <dc:date>2021-07-05T06:44:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148, S32DS CAN Driver Performance Issues.</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-S32DS-CAN-Driver-Performance-Issues/m-p/1308479#M11375</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/13836"&gt;@petervlna&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188029"&gt;@Senlent&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37795"&gt;@lukaszadrapa&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone of you please provide required input?&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jul 2021 14:29:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-S32DS-CAN-Driver-Performance-Issues/m-p/1308479#M11375</guid>
      <dc:creator>Vijay_Arwapally</dc:creator>
      <dc:date>2021-07-15T14:29:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148, S32DS CAN Driver Performance Issues.</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-S32DS-CAN-Driver-Performance-Issues/m-p/1308804#M11381</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;this is what I got from SDK team...&lt;/P&gt;
&lt;P&gt;"The performance of driver’s API depend on different factors (clock, speed rate, payload length, even environment perhaps…). We have &lt;STRONG&gt;no criteria&lt;/STRONG&gt; target for the driver &lt;STRONG&gt;performance&lt;/STRONG&gt; testing. But we had a report about it which was just called profiling report."&lt;/P&gt;
&lt;P&gt;I’ll send you the profiling report of FLEXCAN for RTM 3.0.0 release.&lt;/P&gt;
&lt;P&gt;Hope this will help.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jul 2021 05:13:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-S32DS-CAN-Driver-Performance-Issues/m-p/1308804#M11381</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-07-16T05:13:30Z</dc:date>
    </item>
  </channel>
</rss>