<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Can Tx and Can Rx problem in S32K144 EVB</title>
    <link>https://community.nxp.com/t5/S32K/Can-Tx-and-Can-Rx-problem-in-S32K144-EVB/m-p/1292565#M11155</link>
    <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181122"&gt;@RajG&lt;/a&gt;,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;If there is problem in SBC then also signal on pin should appear right?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;The RX pin must reflect the signal on the TX pin, this is because of synchronization ESR1[SYNCH] and arbitration ESR1[BIT1ERR].&lt;/P&gt;
&lt;P&gt;That's why the PTB1/PTB2 pins must be connected into a loop if they are not connected to any transceiver.&lt;/P&gt;
&lt;P&gt;But now, I understand you can measure some signal on the CAN bus (with the UJA1169 SBC) but it stops if you don't use any delay after a CAN message is sent.&lt;/P&gt;
&lt;P&gt;Is the CAN message acknowledged by another node on the bus?&lt;/P&gt;
&lt;P&gt;The message must be acknowledged otherwise the FlexCAN will keep sending the message until it is acknowledged.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Bosch Controller Area Network (CAN) Version 2.0 PROTOCOL STANDARD&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/BCANPSV2.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/reference-manual/BCANPSV2.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1623757282669.png" style="width: 669px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/147109i99019FB7A8527776/image-dimensions/669x92?v=v2" width="669" height="92" role="button" title="danielmartynek_0-1623757282669.png" alt="danielmartynek_0-1623757282669.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 15 Jun 2021 11:44:47 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2021-06-15T11:44:47Z</dc:date>
    <item>
      <title>Can Tx and Can Rx problem in S32K144 EVB</title>
      <link>https://community.nxp.com/t5/S32K/Can-Tx-and-Can-Rx-problem-in-S32K144-EVB/m-p/1289122#M11090</link>
      <description>&lt;P&gt;Hello all community members, &lt;LI-MESSAGE title="CAN communication not establish in S32K144 EVB" uid="1281751" url="https://community.nxp.com/t5/S32K/CAN-communication-not-establish-in-S32K144-EVB/m-p/1281751#U1281751" discussion_style_icon_css="lia-mention-container-editor-message lia-img-icon-forum-thread lia-fa-icon lia-fa-forum lia-fa-thread lia-fa"&gt;&lt;/LI-MESSAGE&gt;&amp;nbsp;&lt;BR /&gt;I have been trying to do Can communication on s32k144 board with examples provided by SDK itself but have no luck in Signal at output. Examples are&amp;nbsp;flexcan_encrypted_s32k144 and&amp;nbsp;can_pal_s32k144.&lt;/P&gt;&lt;P&gt;I saw waveform on CRO at can high/low along with pin on port PTE4/PTE5 but it is not generating at all.&lt;/P&gt;&lt;P&gt;I also configure another CAN1 bus at port PTA12 and PTA13 still it also didn't show any variation in waveform.&lt;BR /&gt;Given examples is also not working, first i thought SBC problem might be possible but it is not showing any signal on CRO itself.&lt;/P&gt;&lt;P&gt;I tried same thing in MPC5748G development board and i can see can-tx/rx waveform on pin itself.&lt;/P&gt;&lt;P&gt;Kindly help i have been stuck on this since many days,&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;BR /&gt;RajG.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Jun 2021 12:34:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-Tx-and-Can-Rx-problem-in-S32K144-EVB/m-p/1289122#M11090</guid>
      <dc:creator>RajG</dc:creator>
      <dc:date>2021-06-08T12:34:37Z</dc:date>
    </item>
    <item>
      <title>Re: Can Tx and Can Rx problem in S32K144 EVB</title>
      <link>https://community.nxp.com/t5/S32K/Can-Tx-and-Can-Rx-problem-in-S32K144-EVB/m-p/1291383#M11137</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181122"&gt;@RajG&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;There may be something wrong with the SBC.&lt;/P&gt;
&lt;P&gt;Do you power the board with 12V?&lt;/P&gt;
&lt;P&gt;Do you have only one board?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can change the FlexCAN0 ports to PTB0/PTB1&lt;/P&gt;
&lt;P&gt;But you need to connect the two pins externally into a loop.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1623413753368.png" style="width: 800px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146939i813FD9F78DCF5DD6/image-dimensions/800x66?v=v2" width="800" height="66" role="button" title="danielmartynek_0-1623413753368.png" alt="danielmartynek_0-1623413753368.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 07:59:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-Tx-and-Can-Rx-problem-in-S32K144-EVB/m-p/1291383#M11137</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-06-14T07:59:05Z</dc:date>
    </item>
    <item>
      <title>Re: Can Tx and Can Rx problem in S32K144 EVB</title>
      <link>https://community.nxp.com/t5/S32K/Can-Tx-and-Can-Rx-problem-in-S32K144-EVB/m-p/1291607#M11139</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;, thanks for reply,&lt;BR /&gt;If there is problem in SBC then also signal on pin should appear right?&lt;BR /&gt;Yes i have applied external 12V power supply, and I have 1 S32k144 board and 1 MPC5748G board.&lt;BR /&gt;I also have Arduino with MCP2515 shield to check CAN&lt;/P&gt;&lt;P&gt;I did what you suggested, and I found following results:&lt;BR /&gt;1) PTB1 is usually low if not connected to PTB2&lt;BR /&gt;2) PTB2 is usually high if not connected to PTB1&lt;BR /&gt;3) Both PTB1 and PTB2 are high if connected to one another pin.&lt;BR /&gt;4) I can only sense waveform on CRO if I insert some delay after sending Can signal and I can sense it only once. If I reset, I can again see signal.&lt;BR /&gt;The duration is also not fixed, For example i have introduced 1000 millisecond delay then sometime waveform on CRO comes for 3 seconds, sometimes for 5 second and even for 1 sec, its totally random. But it comes only 1 time whenever i reset my board.&lt;BR /&gt;5) If I send Can signal without delay, I find no waveform.&lt;/P&gt;&lt;P&gt;need further assistance,&lt;BR /&gt;Thanks and Regards,&lt;BR /&gt;RajG.&lt;/P&gt;</description>
      <pubDate>Sat, 12 Jun 2021 05:33:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-Tx-and-Can-Rx-problem-in-S32K144-EVB/m-p/1291607#M11139</guid>
      <dc:creator>RajG</dc:creator>
      <dc:date>2021-06-12T05:33:31Z</dc:date>
    </item>
    <item>
      <title>Re: Can Tx and Can Rx problem in S32K144 EVB</title>
      <link>https://community.nxp.com/t5/S32K/Can-Tx-and-Can-Rx-problem-in-S32K144-EVB/m-p/1292565#M11155</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181122"&gt;@RajG&lt;/a&gt;,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;If there is problem in SBC then also signal on pin should appear right?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;The RX pin must reflect the signal on the TX pin, this is because of synchronization ESR1[SYNCH] and arbitration ESR1[BIT1ERR].&lt;/P&gt;
&lt;P&gt;That's why the PTB1/PTB2 pins must be connected into a loop if they are not connected to any transceiver.&lt;/P&gt;
&lt;P&gt;But now, I understand you can measure some signal on the CAN bus (with the UJA1169 SBC) but it stops if you don't use any delay after a CAN message is sent.&lt;/P&gt;
&lt;P&gt;Is the CAN message acknowledged by another node on the bus?&lt;/P&gt;
&lt;P&gt;The message must be acknowledged otherwise the FlexCAN will keep sending the message until it is acknowledged.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Bosch Controller Area Network (CAN) Version 2.0 PROTOCOL STANDARD&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/BCANPSV2.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/reference-manual/BCANPSV2.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1623757282669.png" style="width: 669px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/147109i99019FB7A8527776/image-dimensions/669x92?v=v2" width="669" height="92" role="button" title="danielmartynek_0-1623757282669.png" alt="danielmartynek_0-1623757282669.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Jun 2021 11:44:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-Tx-and-Can-Rx-problem-in-S32K144-EVB/m-p/1292565#M11155</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-06-15T11:44:47Z</dc:date>
    </item>
  </channel>
</rss>