<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image. in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1287615#M11059</link>
    <description>&lt;P&gt;Sorry, missed the jumper reset_b to VSS instruction.&lt;/P&gt;&lt;P&gt;Is the reset_b the same as reset (PTA5)? I couldn't find another reference to it in the IO signal Table.&lt;/P&gt;&lt;P&gt;When I do that I get the following:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;r0
RESET (pin 15) high, but should be low. Please check target hardware.
J-Link&amp;gt;swdwritedp 2,0x01000000
Write DP register 2 = 0x01000000 ***ERROR
J-Link&amp;gt;&lt;/LI-CODE&gt;</description>
    <pubDate>Fri, 04 Jun 2021 14:32:03 GMT</pubDate>
    <dc:creator>lucianomoretti</dc:creator>
    <dc:date>2021-06-04T14:32:03Z</dc:date>
    <item>
      <title>S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1285489#M11021</link>
      <description>&lt;P&gt;I have two S32K144 based boards that we've been working with for the past month and have flashed multiple times. We attempted to program a newly created image with a Cyclone programmer and both targets fail to boot after flash and we're unable to connect to them after the download.&lt;/P&gt;&lt;P&gt;Both targets appeared to program with the Cyclone but immediately after did not boot into the firmware as expected and we are unable to get a SWD connection to the boards using the Cyclone programmers, getting the error $00000007.&lt;/P&gt;&lt;P&gt;I've attempted to connect lowering the shift frequency and adding a delay after reset.&lt;/P&gt;&lt;P&gt;I've attempted to use the PE Micro Kinetis Recovery Tool with no success.&lt;/P&gt;&lt;P&gt;I'm not sure what caused the issues or how to recover. Any assistance isolating the cause and any potential recovery techniques would be appreciated.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jun 2021 14:53:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1285489#M11021</guid>
      <dc:creator>lucianomoretti</dc:creator>
      <dc:date>2021-06-01T14:53:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1286029#M11028</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/46737"&gt;@lucianomoretti&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Can you please scope the reset_b pin (PTA5)?&lt;/P&gt;
&lt;P&gt;Does the MCU keep resetting?&lt;/P&gt;
&lt;P&gt;If so, what is the period of the reset events?&lt;/P&gt;
&lt;P&gt;Do you use CSEc in the application?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 09:36:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1286029#M11028</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-06-02T09:36:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1286188#M11034</link>
      <description>&lt;P&gt;Wow! Yes, the reset line is pulsing every ~113us without a debugger attached when powered up.&lt;/P&gt;&lt;P&gt;As far as I know the application does not use CSEc. It does use the D-Flash region as an emulated EEPROM.&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Reset Line.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146112i4A9323A7680D3CD2/image-size/large?v=v2&amp;amp;px=999" role="button" title="Reset Line.PNG" alt="Reset Line.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Reset Line.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 14:43:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1286188#M11034</guid>
      <dc:creator>lucianomoretti</dc:creator>
      <dc:date>2021-06-02T14:43:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1286817#M11045</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/46737"&gt;@lucianomoretti&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;That means the MCU is reset as soon as it is released from the previous reset.&lt;/P&gt;
&lt;P&gt;The core probably detects an fault exception (leading to core_lookup reset) during the start_up routine.&lt;/P&gt;
&lt;P&gt;It could be because the last loading failed and the flash was left blank or because a wrong image was loaded.&lt;/P&gt;
&lt;P&gt;I'm not sure what the error code means, do you have any other debugger/programmer?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 12:18:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1286817#M11045</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-06-03T12:18:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1286873#M11046</link>
      <description>&lt;P&gt;I've got a J-Link as well as the PE micro programmer (which can be used as a debugger).&lt;/P&gt;&lt;P&gt;I've tried connecting using the J-Link and J-Flash but it pulls up the popup stating that the "Protection bytes in flash addr. 0x400-0x40F indicate that readout protection is set" and trying to clear it does not work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Application log started
 - J-Flash V6.94d (J-Flash compiled Feb 12 2021 15:53:19)
 - JLinkARM.dll V6.94d (DLL compiled Feb 12 2021 15:52:57)
Reading flash device list [C:\Program Files (x86)\SEGGER\JLink\ETC/JFlash/Flash.csv] ...
 - List of flash devices read successfully (451 Devices)
Reading MCU device list ...
 - List of MCU devices read successfully (8145 Devices)
Opening project file [C:\Users\DEVELOP-LLC\MCM_S32.jflash] ...
 - Project opened successfully
No data file specified!
Failed to open data file [C:\Users\DEVELOP-LLC\]...
Connecting ...
 - Connecting via USB to probe/ programmer device 0
 - Probe/ Programmer firmware: J-Link V11 compiled Feb  4 2021 12:59:17
 - Device "S32K144 (ALLOW SECURITY)" selected.
 - Target interface speed: 4000 kHz (Fixed)
 - VTarget = 5.019V
 - InitTarget() start
 - InitTarget()
 - Device will be unsecured now.
 - Timeout while unsecuring device. Erase never stops.
 - InitTarget() end
 - Found SW-DP with ID 0x2BA01477
 - DPIDR: 0x2BA01477
 - Scanning AP map to find all available APs
 - AP[2]: Stopped AP scan as end of AP map has been reached
 - AP[0]: AHB-AP (IDR: 0x24770011)
 - AP[1]: JTAG-AP (IDR: 0x001C0000)
 - Iterating through AP map to find AHB-AP to use
 - AP[0]: Skipped. Could not read CPUID register
 - AP[1]: Skipped. Not an AHB-AP
 - InitTarget() start
 - InitTarget()
 - Device will be unsecured now.
 - Timeout while unsecuring device. Erase never stops.
 - InitTarget() end
 - Found SW-DP with ID 0x2BA01477
 - DPIDR: 0x2BA01477
 - Scanning AP map to find all available APs
 - AP[2]: Stopped AP scan as end of AP map has been reached
 - AP[0]: AHB-AP (IDR: 0x24770011)
 - AP[1]: JTAG-AP (IDR: 0x001C0000)
 - Iterating through AP map to find AHB-AP to use
 - AP[0]: Skipped. Could not read CPUID register
 - AP[1]: Skipped. Not an AHB-AP
 - ERROR: Could not find core in Coresight setup
 - ERROR: Failed to connect.
Could not establish a connection to target.&lt;/LI-CODE&gt;</description>
      <pubDate>Thu, 03 Jun 2021 13:34:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1286873#M11046</guid>
      <dc:creator>lucianomoretti</dc:creator>
      <dc:date>2021-06-03T13:34:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1287016#M11047</link>
      <description>&lt;P&gt;I scoped the reset line while trying to communicate with the debugger and while the probe is accessing the system the reset line remains low.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 19:18:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1287016#M11047</guid>
      <dc:creator>lucianomoretti</dc:creator>
      <dc:date>2021-06-03T19:18:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1287476#M11056</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Can you please connect the reset_b pin to VSS and power cycle the MCU so that the MCU can stay in reset after POR?&lt;/P&gt;
&lt;P&gt;Then read the MDM-AP Status register and try the Unlock Kinetis command in J-link commander.&lt;/P&gt;
&lt;P&gt;If the unlock command is successful, try loading an S32K144 example from the S32DS IDE.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;r0                      // pull reset pin low

J-Link&amp;gt;swdwritedp 2,0x01000000 // MDM_AP status register

J-Link&amp;gt;swdreadap 0      // Read MDM_AP status register
J-Link&amp;gt;swdreadap 0      // Read MDM_AP status register (has to be done 2x) Flash memory ready and Mass erase enable bits should be set

J-Link&amp;gt;swdreadap 1      // Read MDM_AP control register
J-Link&amp;gt;swdreadap 1      // Read MDM_AP control register (has to be done 2x) 

J-Link&amp;gt;unlock Kinetis   // Erase and unsecure the MCU
 ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 10:27:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1287476#M11056</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-06-04T10:27:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1287605#M11058</link>
      <description>&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;r0
J-Link&amp;gt;swdwritedp 2,0x01000000
Write DP register 2 = 0x01000000 ***ERROR&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Didn't like that.&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 14:17:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1287605#M11058</guid>
      <dc:creator>lucianomoretti</dc:creator>
      <dc:date>2021-06-04T14:17:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1287615#M11059</link>
      <description>&lt;P&gt;Sorry, missed the jumper reset_b to VSS instruction.&lt;/P&gt;&lt;P&gt;Is the reset_b the same as reset (PTA5)? I couldn't find another reference to it in the IO signal Table.&lt;/P&gt;&lt;P&gt;When I do that I get the following:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;r0
RESET (pin 15) high, but should be low. Please check target hardware.
J-Link&amp;gt;swdwritedp 2,0x01000000
Write DP register 2 = 0x01000000 ***ERROR
J-Link&amp;gt;&lt;/LI-CODE&gt;</description>
      <pubDate>Fri, 04 Jun 2021 14:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1287615#M11059</guid>
      <dc:creator>lucianomoretti</dc:creator>
      <dc:date>2021-06-04T14:32:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1288245#M11069</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/46737"&gt;@lucianomoretti&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Yes, PTA5 is reset_b.&lt;/P&gt;
&lt;P&gt;Did you connect it to VSS (ground) or VDD?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jun 2021 11:08:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1288245#M11069</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-06-07T11:08:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1288501#M11074</link>
      <description>&lt;P&gt;I connected to VDD, not VSS. I tried again connecting to VSS and got the following:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;r0
J-Link&amp;gt;swdwritedp 2,0x01000000
Write DP register 2 = 0x01000000 ***ERROR
J-Link&amp;gt;&lt;/LI-CODE&gt;</description>
      <pubDate>Mon, 07 Jun 2021 18:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1288501#M11074</guid>
      <dc:creator>lucianomoretti</dc:creator>
      <dc:date>2021-06-07T18:15:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1289848#M11105</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/46737"&gt;@lucianomoretti&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I haven't met this kind of error.&lt;/P&gt;
&lt;P&gt;Can you show the whole log from the commander?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 10:47:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1289848#M11105</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-06-09T10:47:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1292006#M11145</link>
      <description>&lt;P&gt;Unfortunately, as we needed to keep moving forward we swapped the dead chip out for a new one. So far we have been successfully programming the device with new images.&lt;/P&gt;&lt;P&gt;If you want the chip for analysis I could probably get it shipped to someone but it's currently not on a PCB.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 14:49:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1292006#M11145</guid>
      <dc:creator>lucianomoretti</dc:creator>
      <dc:date>2021-06-14T14:49:13Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Board does not boot/cannot connect SWD after flashing with Cyclone image.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1294119#M11174</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/46737"&gt;@lucianomoretti&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Unfortunately, this is out of my responsibility.&lt;/P&gt;
&lt;P&gt;The only option to initiate a failure analysis is to contact your point of sales.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/company/about-nxp/quality/product-analysis:QUALITY_PRD_ANALYSIS" target="_blank"&gt;https://www.nxp.com/company/about-nxp/quality/product-analysis:QUALITY_PRD_ANALYSIS&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jun 2021 13:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Board-does-not-boot-cannot-connect-SWD-after-flashing/m-p/1294119#M11174</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-06-17T13:17:00Z</dc:date>
    </item>
  </channel>
</rss>