<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Estimated RPM and speed in MCSPTE1AK144 FOC PMSM application in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Estimated-RPM-and-speed-in-MCSPTE1AK144-FOC-PMSM-application/m-p/1285474#M11019</link>
    <description>&lt;P&gt;Hello to all, I wanted to send the current RPM and speed of the motor in MCSPTE1AK144 kit via UART to console for my application.&lt;/P&gt;&lt;P&gt;From the code provide of 2 resistor sense PMSM FOC based software, I am writing value to "drvFOC.pospeControl.wRotElReq" structure for rotation of motor. Here&amp;nbsp;wRotElReq is the required speed variable, so we can change it to get specific rpm.&lt;/P&gt;&lt;P&gt;I would like to know the calculated/ estimated speed and RPM of the motor so i can transmit it via UART and have a feedback value about the rotation. I kindly request to help me with some variable or structure which i dont know in this code that can directly give such estimated RPM and speed.&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;RajG.&lt;/P&gt;</description>
    <pubDate>Tue, 01 Jun 2021 14:28:31 GMT</pubDate>
    <dc:creator>RajG</dc:creator>
    <dc:date>2021-06-01T14:28:31Z</dc:date>
    <item>
      <title>Estimated RPM and speed in MCSPTE1AK144 FOC PMSM application</title>
      <link>https://community.nxp.com/t5/S32K/Estimated-RPM-and-speed-in-MCSPTE1AK144-FOC-PMSM-application/m-p/1285474#M11019</link>
      <description>&lt;P&gt;Hello to all, I wanted to send the current RPM and speed of the motor in MCSPTE1AK144 kit via UART to console for my application.&lt;/P&gt;&lt;P&gt;From the code provide of 2 resistor sense PMSM FOC based software, I am writing value to "drvFOC.pospeControl.wRotElReq" structure for rotation of motor. Here&amp;nbsp;wRotElReq is the required speed variable, so we can change it to get specific rpm.&lt;/P&gt;&lt;P&gt;I would like to know the calculated/ estimated speed and RPM of the motor so i can transmit it via UART and have a feedback value about the rotation. I kindly request to help me with some variable or structure which i dont know in this code that can directly give such estimated RPM and speed.&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;RajG.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jun 2021 14:28:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Estimated-RPM-and-speed-in-MCSPTE1AK144-FOC-PMSM-application/m-p/1285474#M11019</guid>
      <dc:creator>RajG</dc:creator>
      <dc:date>2021-06-01T14:28:31Z</dc:date>
    </item>
    <item>
      <title>Re: Estimated RPM and speed in MCSPTE1AK144 FOC PMSM application</title>
      <link>https://community.nxp.com/t5/S32K/Estimated-RPM-and-speed-in-MCSPTE1AK144-FOC-PMSM-application/m-p/1287808#M11063</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52961"&gt;@PetrS&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/134742"&gt;@marekmusak&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;stuck since many days and no one replied to my query, so tagging you all sir,&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;BR /&gt;RajG.&lt;/P&gt;</description>
      <pubDate>Sat, 05 Jun 2021 10:18:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Estimated-RPM-and-speed-in-MCSPTE1AK144-FOC-PMSM-application/m-p/1287808#M11063</guid>
      <dc:creator>RajG</dc:creator>
      <dc:date>2021-06-05T10:18:54Z</dc:date>
    </item>
    <item>
      <title>Re: Estimated RPM and speed in MCSPTE1AK144 FOC PMSM application</title>
      <link>https://community.nxp.com/t5/S32K/Estimated-RPM-and-speed-in-MCSPTE1AK144-FOC-PMSM-application/m-p/1294049#M11172</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hello RajG,&lt;/P&gt;
&lt;P&gt;To get actual rotor speed, use variable&amp;nbsp;drvFOC.pospeControl.wRotEl which is an electrical speed in format rad/s.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To get speed in rpm format, it must be multiplied by (60/2*pi*pp), where pp is number of pope pairs. Motor of this kit has two pole pairs, thus pp=2.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;FreeMASTER variable "Speed FOC loop" has the same RPM format.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Marek&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jun 2021 10:42:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Estimated-RPM-and-speed-in-MCSPTE1AK144-FOC-PMSM-application/m-p/1294049#M11172</guid>
      <dc:creator>marekmusak</dc:creator>
      <dc:date>2021-06-17T10:42:25Z</dc:date>
    </item>
  </channel>
</rss>