<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Watchdog Rest After Sleep/Wake-Up in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284770#M11005</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for quick response.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. I am using VLPR and then VLPS because perrodic wake-up is not happening (for VLPR I used your previously shared code for perodic wake-up).&lt;/P&gt;&lt;P&gt;2. After wake-up watchdog not re-initialized then LIN is not working.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;POWER_SYS_GetResetSrcStatusCmd(RCM, RCM_WATCH_DOG); this to check watchdog reset.&lt;/P&gt;&lt;P&gt;But when I checked register of watchog in ide there is no change in registers after wake-up from sleep.&lt;/P&gt;&lt;P&gt;I am checking below registers. for watchdog.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="chaitanya_kalya_0-1622460639613.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145884i8A29C37E6298E272/image-size/medium?v=v2&amp;amp;px=400" role="button" title="chaitanya_kalya_0-1622460639613.png" alt="chaitanya_kalya_0-1622460639613.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Before and after wake-up from sleep value on these register is same. But when I read for watchdog reset then getting watchdog reset.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 31 May 2021 11:35:47 GMT</pubDate>
    <dc:creator>chaitanya_kalyani</dc:creator>
    <dc:date>2021-05-31T11:35:47Z</dc:date>
    <item>
      <title>Watchdog Rest After Sleep/Wake-Up</title>
      <link>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284409#M10998</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using S32K116 for our one of the project. I have implemented perodic wake-up and when it comes fully run mode from perodic wake-up watchdog reset is happening after wake-up. When it start and before enter into sleep watchdog reset is not showing but issue is when enter into sleep.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Before entering into sleep I am disabling the watchdog still watchdog reset is happening.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using below settings.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="chaitanya_kalya_0-1622373313124.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145839i9995E5FF99E5D2C5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="chaitanya_kalya_0-1622373313124.png" alt="chaitanya_kalya_0-1622373313124.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I am using below code to enter into sleep&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;void GoToSleep(void)&lt;BR /&gt;{&lt;BR /&gt;INT_SYS_DisableIRQGlobal();&lt;BR /&gt;&lt;BR /&gt;INT_SYS_DisableIRQ(WDOG_IRQn);&lt;BR /&gt;WDOG_DRV_Deinit(INST_WATCHDOG1);&lt;BR /&gt;PINS_DRV_SetPinIntSel(PORTC,2,PORT_INT_FALLING_EDGE);&lt;BR /&gt;INT_SYS_EnableIRQ(PORT_IRQn);&lt;BR /&gt;//Deinit LPIT&lt;BR /&gt;LPIT_DRV_StopTimerChannels(INST_TIMER1MS,&amp;nbsp;(1 &amp;lt;&amp;lt; TIMER_1MS_CHANNEL));&lt;BR /&gt;LowPowerModeLPTMR();&lt;BR /&gt;INT_SYS_EnableIRQGlobal();&lt;BR /&gt;//Enter to VLPS&lt;BR /&gt;enter_VLPR();&lt;BR /&gt;POWER_SYS_SetMode(VLPS,POWER_MANAGER_POLICY_AGREEMENT);&lt;BR /&gt;VLPS_To_Run();&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;static void VLPS_To_Run(void)&lt;BR /&gt;{&lt;BR /&gt;//Start Run Mode&lt;BR /&gt;POWER_SYS_SetMode(RUN,&amp;nbsp;POWER_MANAGER_POLICY_AGREEMENT);&lt;BR /&gt;RunModeLPTMR();&lt;BR /&gt;PINS_DRV_SetPinIntSel(PORTC, 2,&amp;nbsp;PORT_DMA_INT_DISABLED);&lt;BR /&gt;INT_SYS_DisableIRQ(PORT_IRQn);&lt;BR /&gt;//LPTMR&lt;BR /&gt;LPTMR_DRV_Init(INST_LPTMR,&amp;nbsp;&amp;amp;lpTmr_config0,&amp;nbsp;false);&lt;BR /&gt;INT_SYS_EnableIRQ(LPTMR0_IRQn);&lt;BR /&gt;LPTMR_DRV_StartCounter(INST_LPTMR);&lt;/P&gt;&lt;P&gt;//Start Watchdog&lt;BR /&gt;WDOG_DRV_Init(INST_WATCHDOG1,&amp;nbsp;&amp;amp;watchdog1_Config0);&lt;BR /&gt;INT_SYS_EnableIRQGlobal();&lt;/P&gt;&lt;P&gt;//Start LPIT&lt;BR /&gt;LPIT_DRV_StartTimerChannels(INST_TIMER1MS,&amp;nbsp;(1 &amp;lt;&amp;lt; TIMER_1MS_CHANNEL));&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Triggering watchdog in LPTMR ISR and using&amp;nbsp;POWER_SYS_GetResetSrcStatusCmd(RCM, RCM_WATCH_DOG) this to check it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In Perodic wake-up also I am triggering the watchdog still watchdog reset is happening.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 30 May 2021 11:23:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284409#M10998</guid>
      <dc:creator>chaitanya_kalyani</dc:creator>
      <dc:date>2021-05-30T11:23:28Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog Rest After Sleep/Wake-Up</title>
      <link>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284702#M11002</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/94876"&gt;@chaitanya_kalyani&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Can you please share the project.&lt;/P&gt;
&lt;P&gt;I don't think I can find the root cause just from the description.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 31 May 2021 09:48:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284702#M11002</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-05-31T09:48:54Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog Rest After Sleep/Wake-Up</title>
      <link>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284731#M11003</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Project sharing is not possible.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In this project I am using LIN as communication and as previously you suggested LPTMR for perodic wake-up. Thus issue only when it is enter into sleep and wake-up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;</description>
      <pubDate>Mon, 31 May 2021 10:34:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284731#M11003</guid>
      <dc:creator>chaitanya_kalyani</dc:creator>
      <dc:date>2021-05-31T10:34:56Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog Rest After Sleep/Wake-Up</title>
      <link>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284740#M11004</link>
      <description>&lt;P&gt;If the MCU is reset by the WDOG, the code is probably stuck somewhere in the RUN mode after the WDOG gets reinitialized.&lt;/P&gt;
&lt;P&gt;Maybe you can left the WDOG disabled after the wake-up and measure the time between WDOG refresh events by toggling a GPIO.&lt;/P&gt;
&lt;P&gt;Why the application enters VLPR before it goes to VLPS?&lt;/P&gt;
&lt;P&gt;It can go from RUN to VLPS directly.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 31 May 2021 10:48:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284740#M11004</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-05-31T10:48:11Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog Rest After Sleep/Wake-Up</title>
      <link>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284770#M11005</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for quick response.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. I am using VLPR and then VLPS because perrodic wake-up is not happening (for VLPR I used your previously shared code for perodic wake-up).&lt;/P&gt;&lt;P&gt;2. After wake-up watchdog not re-initialized then LIN is not working.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;POWER_SYS_GetResetSrcStatusCmd(RCM, RCM_WATCH_DOG); this to check watchdog reset.&lt;/P&gt;&lt;P&gt;But when I checked register of watchog in ide there is no change in registers after wake-up from sleep.&lt;/P&gt;&lt;P&gt;I am checking below registers. for watchdog.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="chaitanya_kalya_0-1622460639613.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145884i8A29C37E6298E272/image-size/medium?v=v2&amp;amp;px=400" role="button" title="chaitanya_kalya_0-1622460639613.png" alt="chaitanya_kalya_0-1622460639613.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Before and after wake-up from sleep value on these register is same. But when I read for watchdog reset then getting watchdog reset.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 31 May 2021 11:35:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284770#M11005</guid>
      <dc:creator>chaitanya_kalyani</dc:creator>
      <dc:date>2021-05-31T11:35:47Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog Rest After Sleep/Wake-Up</title>
      <link>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284775#M11006</link>
      <description>&lt;P&gt;HI &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/94876"&gt;@chaitanya_kalyani&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I would recommend using the POWER_SYS_SetMode() function for VLPR as well.&lt;/P&gt;
&lt;P&gt;But as I said, there is no need to go to VLPR first if the application does not need to run in VLPR.&lt;/P&gt;
&lt;P&gt;Also, the LPTMR must run in VLPS regardless of the previous RUN/VLPR mode.&lt;/P&gt;
&lt;P&gt;Can you simply read the RCM_SRS register at the beginning of main() and send the value out?&lt;/P&gt;
&lt;P&gt;The MCU should run stand-alone in VLPS without the debugger.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 31 May 2021 11:52:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284775#M11006</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-05-31T11:52:09Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog Rest After Sleep/Wake-Up</title>
      <link>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284781#M11007</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I use&amp;nbsp;&lt;SPAN&gt;POWER_SYS_SetMode() for VLPR also then also getting problem for perodic wake-up. The code that you have provided for VLPR that only working.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;On RCM_SRS register watdog value is getting set after wake-up from sleep mode. Before enter into sleep it is 64 and after wake-up from sleep it is becoming 32 that is watchdog bit is getting set. It is not getting set in sleep mode it is getting se only after wake-up.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have one more question if watchdog reset is happened then if we do reset that will impact on anything. Is it good of we do software reset if watchdog reset is happened ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 31 May 2021 12:13:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1284781#M11007</guid>
      <dc:creator>chaitanya_kalyani</dc:creator>
      <dc:date>2021-05-31T12:13:39Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog Rest After Sleep/Wake-Up</title>
      <link>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1286809#M11044</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/94876"&gt;@chaitanya_kalyani&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The code that I provided for VLPR does a few things that are needed for VLPS as well.&lt;/P&gt;
&lt;P&gt;The enter_VLPR() function switches the system clock to SIRC, allows VLP* operation etc.&lt;/P&gt;
&lt;P&gt;Maybe you haven't enabled SIRC in VLPS in the PE configuration.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The RCM_SRS gets set during the system reset to indicate the source of the reset.&lt;/P&gt;
&lt;P&gt;If the WDOG bit is set, the MCU has been reset by the WDOG after the wakeup and after the WDOG was enabled.&lt;/P&gt;
&lt;P&gt;As I said, the program must be stuck somewhere, the WDOG is not being fed and it resets the MCU.&lt;/P&gt;
&lt;P&gt;Please leave the WDOG disabled after the wakeup and find out where it is stuck.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The WDOG resets the MCU, there is no need for an additional reset.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 12:07:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Watchdog-Rest-After-Sleep-Wake-Up/m-p/1286809#M11044</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-06-03T12:07:32Z</dc:date>
    </item>
  </channel>
</rss>