<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Delay of LPSPI between frames in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Delay-of-LPSPI-between-frames/m-p/1283872#M10989</link>
    <description>&lt;P&gt;Regarding to the delay such PCSSCK, SCKPCS and DBT of S32K144 LPSPI CCR, SCKPCS in reference manual states "configures the delay from the last SCK edge to the PCS negation".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Even without PCS negation between frames, do the delays occur correctly?&lt;/P&gt;&lt;P&gt;When CS has been kept assertion between frames using GPIO, it seemed ​like the delays occurred.&lt;/P&gt;</description>
    <pubDate>Fri, 28 May 2021 05:09:07 GMT</pubDate>
    <dc:creator>fumiaki</dc:creator>
    <dc:date>2021-05-28T05:09:07Z</dc:date>
    <item>
      <title>Delay of LPSPI between frames</title>
      <link>https://community.nxp.com/t5/S32K/Delay-of-LPSPI-between-frames/m-p/1283872#M10989</link>
      <description>&lt;P&gt;Regarding to the delay such PCSSCK, SCKPCS and DBT of S32K144 LPSPI CCR, SCKPCS in reference manual states "configures the delay from the last SCK edge to the PCS negation".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Even without PCS negation between frames, do the delays occur correctly?&lt;/P&gt;&lt;P&gt;When CS has been kept assertion between frames using GPIO, it seemed ​like the delays occurred.&lt;/P&gt;</description>
      <pubDate>Fri, 28 May 2021 05:09:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Delay-of-LPSPI-between-frames/m-p/1283872#M10989</guid>
      <dc:creator>fumiaki</dc:creator>
      <dc:date>2021-05-28T05:09:07Z</dc:date>
    </item>
    <item>
      <title>Re: Delay of LPSPI between frames</title>
      <link>https://community.nxp.com/t5/S32K/Delay-of-LPSPI-between-frames/m-p/1283942#M10991</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/187261"&gt;@fumiaki&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The LPSPI module does not have an option to disable the PCS.&lt;/P&gt;
&lt;P&gt;So even if you don't use the PCS output of the LPSPI module on a port but you use a GPIO instead, the module still keeps generating it with the configurable delay.&amp;nbsp; &amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Fri, 28 May 2021 07:08:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Delay-of-LPSPI-between-frames/m-p/1283942#M10991</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-05-28T07:08:43Z</dc:date>
    </item>
  </channel>
</rss>