<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: s32k144 FTM_SignalMeasurement_Example can not work</title>
    <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687297#M1096</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi rares&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you give me you use example ,i could not use also&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Jul 2017 08:09:07 GMT</pubDate>
    <dc:creator>jiangbolwj</dc:creator>
    <dc:date>2017-07-11T08:09:07Z</dc:date>
    <item>
      <title>s32k144 FTM_SignalMeasurement_Example can not work</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687291#M1090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i use this example to test the singnal mesaurement but i can not capture the singal , alwy is one point,i find this program can not into the interrupt,can you help me&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 00:20:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687291#M1090</guid>
      <dc:creator>jiangbolwj</dc:creator>
      <dc:date>2017-07-07T00:20:17Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 FTM_SignalMeasurement_Example can not work</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687292#M1091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24859iCED181E4F0B5530D/image-size/large?v=v2&amp;amp;px=999" title="QQ截图20170707141140.png" alt="QQ截图20170707141140.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #666666; background-color: rgba(255, 255, 255, 0.8); font-size: 12px;"&gt;By using data obtained from a serial port tool as shown&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 06:14:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687292#M1091</guid>
      <dc:creator>jiangbolwj</dc:creator>
      <dc:date>2017-07-07T06:14:19Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 FTM_SignalMeasurement_Example can not work</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687293#M1092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Was the connection between the FTM0 PWM pin and FTM1 IC pin done correctly?(Please consult the example documentation for the information about the connection).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What version of the SDK are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Rares&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 07:25:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687293#M1092</guid>
      <dc:creator>raresvasile</dc:creator>
      <dc:date>2017-07-07T07:25:59Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 FTM_SignalMeasurement_Example can not work</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687294#M1093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;FTM0 is PTC0 FTM1 is PTCB2 the point is right ,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I use SDK is 1.3&amp;nbsp; using the example is SDK v1.0&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 07:32:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687294#M1093</guid>
      <dc:creator>jiangbolwj</dc:creator>
      <dc:date>2017-07-07T07:32:36Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 FTM_SignalMeasurement_Example can not work</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687295#M1094</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that there is a typo in the documentation of the example.&lt;/P&gt;&lt;P&gt;Instead of J3-11 you need to connect to J4-11. So the connection would be PTC0(J4-11) -&amp;gt; PTB2(J2-11).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried the example on RTM and it worked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Rares&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 07:44:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687295#M1094</guid>
      <dc:creator>raresvasile</dc:creator>
      <dc:date>2017-07-07T07:44:49Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 FTM_SignalMeasurement_Example can not work</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687296#M1095</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i try but not ok&lt;/P&gt;&lt;P&gt;i write one to look if it &amp;nbsp;can into the interrupt ,it can not into the intterrupt ,can you help me have a look &amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Jul 2017 03:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687296#M1095</guid>
      <dc:creator>jiangbolwj</dc:creator>
      <dc:date>2017-07-08T03:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 FTM_SignalMeasurement_Example can not work</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687297#M1096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi rares&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you give me you use example ,i could not use also&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 08:09:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687297#M1096</guid>
      <dc:creator>jiangbolwj</dc:creator>
      <dc:date>2017-07-11T08:09:07Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 FTM_SignalMeasurement_Example can not work</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687298#M1097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I modified the project and it is working. Please find it attached.&lt;/P&gt;&lt;P&gt;I updated the following: &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;- FTM clock source to System Clock in it's PEx component. In the original project it was using External Clock, which should be provided from an external source.&lt;/P&gt;&lt;P&gt;&amp;nbsp;- Removed interrupt installation from main and assigned&amp;nbsp;FTM1_ch3_Input_Capture_isr&amp;nbsp;as a callback for the FTM IC channel 0. FTM driver uses hardware interrupts to process measurements and calls user callbacks which are configurable for each channel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Rares&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 11:30:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687298#M1097</guid>
      <dc:creator>raresvasile</dc:creator>
      <dc:date>2017-07-11T11:30:28Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 FTM_SignalMeasurement_Example can not work</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687299#M1098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i try but not succeess&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i read the&amp;nbsp;&lt;SPAN style="color: #434343; background-color: #f2f2f2; font-size: 12px;"&gt;register ,the register of capture flag have bit 1, the flag of interrupt have bit of 1,but it could not into the interrutpt&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #434343; background-color: #f2f2f2; font-size: 12px;"&gt;if the board&amp;nbsp; i am used is break, i ues board is FRDM-s32k144&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25735i3AB831B0DA2D0AFF/image-size/large?v=v2&amp;amp;px=999" title="QQ截图20170712110709.png" alt="QQ截图20170712110709.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25774i9EDFDCFEB77060E4/image-size/large?v=v2&amp;amp;px=999" title="QQ截图20170712110805.png" alt="QQ截图20170712110805.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #434343; background-color: #f2f2f2; font-size: 12px;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25812i2FA1FB94745AF57A/image-size/large?v=v2&amp;amp;px=999" title="QQ截图20170712111716.png" alt="QQ截图20170712111716.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2017 03:26:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687299#M1098</guid>
      <dc:creator>jiangbolwj</dc:creator>
      <dc:date>2017-07-12T03:26:13Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 FTM_SignalMeasurement_Example can not work</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687300#M1099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The latest S32DS and SDKs supports the latest MCU revisions. These are mounted on S32K144EVB-Q100. The FRDM board has MCU with first revision (mask 0N77P) mounted. There are differences in vector table, that’s why the example is not working on your board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The S32 sdk ear 0.8.1 supports cut1 MCU (mask 0N77P) and its demo example FTM_SignalMeasurement_Example works well on the FRDM board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I guess this earlier SDK versions are not maintained anymore and it is advisable to use the &lt;SPAN&gt;S32K144EVB-Q100 with latest S32DS and SDKs versions.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;It could be also possible to assign correct ISR vector in the driver, but this is not recommended way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2017 08:27:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-FTM-SignalMeasurement-Example-can-not-work/m-p/687300#M1099</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-07-12T08:27:48Z</dc:date>
    </item>
  </channel>
</rss>