<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K146 CAN FD in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K146-CAN-FD/m-p/1281506#M10944</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;use crystal with higher frequency or select system clock as PE clock source.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Tue, 25 May 2021 05:59:17 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2021-05-25T05:59:17Z</dc:date>
    <item>
      <title>S32K146 CAN FD</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-CAN-FD/m-p/1277669#M10896</link>
      <description>&lt;P&gt;Q1: CAN-FD data phase only set max 1000kbit/s ？&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q2 : CAN-FD:&lt;/P&gt;&lt;P&gt;if the CAN bus is connected when the machine is started, the transceiver is normal;&lt;/P&gt;&lt;P&gt;but cannot send out data return BUSY while hot-plug.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="token keyword"&gt;if&lt;/SPAN&gt; &lt;SPAN class="token punctuation"&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;state&lt;/SPAN&gt;&lt;SPAN class="token operator"&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;mbs&lt;/SPAN&gt;&lt;SPAN class="token punctuation"&gt;[&lt;/SPAN&gt;&lt;SPAN&gt;mb_idx&lt;/SPAN&gt;&lt;SPAN class="token punctuation"&gt;]&lt;/SPAN&gt;&lt;SPAN class="token punctuation"&gt;.&lt;/SPAN&gt;&lt;SPAN&gt;state &lt;/SPAN&gt;&lt;SPAN class="token operator"&gt;!=&lt;/SPAN&gt;&lt;SPAN&gt; FLEXCAN_MB_IDLE&lt;/SPAN&gt;&lt;SPAN class="token punctuation"&gt;)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="token punctuation"&gt;{&lt;/SPAN&gt; &lt;SPAN class="token keyword"&gt;return&lt;/SPAN&gt;&lt;SPAN&gt; STATUS_BUSY&lt;/SPAN&gt;&lt;SPAN class="token punctuation"&gt;;&lt;/SPAN&gt; &lt;SPAN class="token punctuation"&gt;}&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 17 May 2021 14:40:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-CAN-FD/m-p/1277669#M10896</guid>
      <dc:creator>gravity_one</dc:creator>
      <dc:date>2021-05-17T14:40:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 CAN FD</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-CAN-FD/m-p/1278092#M10899</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1) theoretically up to 8Mbps is supported, but this is also limited by used PE clock, transceiver and real bus.&lt;/P&gt;
&lt;P&gt;2) there should not be problem with hot-plug. If the MB cannot still be used for transmission, try to first AbortTransfer and then send message normally.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 May 2021 08:38:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-CAN-FD/m-p/1278092#M10899</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-05-18T08:38:05Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 CAN FD</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-CAN-FD/m-p/1278889#M10909</link>
      <description>&lt;P&gt;hello，&lt;/P&gt;&lt;P&gt;set Data phase to MAX 1600kbit/s by ProcessorExpert.pe&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1621418426(1).png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145043i8B3D69149C9C14D6/image-size/large?v=v2&amp;amp;px=999" role="button" title="1621418426(1).png" alt="1621418426(1).png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1621418426(1).png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 10:01:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-CAN-FD/m-p/1278889#M10909</guid>
      <dc:creator>gravity_one</dc:creator>
      <dc:date>2021-05-19T10:01:10Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 CAN FD</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-CAN-FD/m-p/1281506#M10944</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;use crystal with higher frequency or select system clock as PE clock source.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 25 May 2021 05:59:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-CAN-FD/m-p/1281506#M10944</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-05-25T05:59:17Z</dc:date>
    </item>
  </channel>
</rss>