<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K144EVB CAN transceiver with NXP example model</title>
    <link>https://community.nxp.com/t5/S32K/S32K144EVB-CAN-transceiver-with-NXP-example-model/m-p/1279042#M10916</link>
    <description>&lt;P&gt;Solved, by taping some iffy CAN cable connections together.&lt;LI-EMOJI id="lia_fearful-face" title=":fearful_face:"&gt;&lt;/LI-EMOJI&gt; &amp;nbsp;I'm going to mark your answer,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57959"&gt;@Robin_Shen&lt;/a&gt;, as the correct one, however, so people can find the helpful info.&lt;/P&gt;</description>
    <pubDate>Wed, 19 May 2021 14:26:40 GMT</pubDate>
    <dc:creator>neffnan</dc:creator>
    <dc:date>2021-05-19T14:26:40Z</dc:date>
    <item>
      <title>S32K144EVB CAN transceiver with NXP example model</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-CAN-transceiver-with-NXP-example-model/m-p/1278486#M10903</link>
      <description>&lt;P&gt;I am trying to run the NXP MBDT CAN example titled "CAN_Traffic", model flexcan_s32k14x.slx, on the evaluation board S32K144EVB-Q100. I am using MATLAB/Simulink 2020a, and version 4.2.0 of NXP's MBDT. The physical configuration is:&lt;/P&gt;&lt;P&gt;- board is powered by 12VDC to the J16 connector (the jumper on J107 is on pins 1-2)&lt;BR /&gt;- CAN cable from the CAN connector on the board to a Y-splitter&lt;BR /&gt;- one arm of the Y is connected via a Vector VN1630A CANcase to a USB port on the PC&lt;BR /&gt;- the other arm of the Y is connected to a PEAK PCAN-USB, which is connected to another USB port on the PC&lt;/P&gt;&lt;P&gt;I am running Peak's PCAN-View and Vector's CANalyzer on the PC, and transmitting the message required by the NXP example model, ID 0x3FE, from PCAN-View.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I ran this setup yesterday, with an evaluation board with the UJA1169 disabled and a different transceiver (TI&amp;nbsp;SN65HVD230Q, if it matters)&amp;nbsp;wired up externally, everything worked exactly as advertised.&lt;/P&gt;&lt;P&gt;Today, with exactly the same test hardware and cabling, plus a brand-new evaluation board (with the UJA1169 untouched), I'm getting no traffic on the CAN bus. PCAN-View reports that bus Status is "OK" and the red LED on the board is on when everything is first powered up, but when I start transmitting msg 0x3FE from PCAN-View, the bus Status in PCAN-View changes to "BUS-OFF", neither CANalyzer nor PCAN-View show any bus traffic, and the red LED is not blinking. (I have the cycle time long enough on the transmission of msg 0x3FE that I saw the blinking quite clearly yesterday, so I know the board is not seeing 0x3FE today.)&lt;/P&gt;&lt;P&gt;So the NXP CAN_Traffic example model worked with the TI transceiver yesterday but is not working with the UJA1169 on an unmodified board today, with otherwise exactly the same setup.&lt;/P&gt;&lt;P&gt;I'd appreciate any help anyone can offer. Thanks. --Nancy&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 00:21:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-CAN-transceiver-with-NXP-example-model/m-p/1278486#M10903</guid>
      <dc:creator>neffnan</dc:creator>
      <dc:date>2021-05-19T00:21:52Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB CAN transceiver with NXP example model</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-CAN-transceiver-with-NXP-example-model/m-p/1278550#M10906</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Nancy,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;The MBDT is currently supported on our &lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/bd-p/mbdt" target="_self"&gt;community&lt;/A&gt; only.&lt;BR /&gt;If I am not able to help you find out the issue, maybe you need to post the questions there.&lt;BR /&gt;The community is monitored by our experts on the tools.&lt;BR /&gt;I'm sorry for the inconvenience.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Would you please let me know the version of S32K144EVB?&lt;BR /&gt;For the &lt;STRONG&gt;RevC&lt;/STRONG&gt; version, the J107 should connect 2-3.(External 12V power\ using CAN transceiver of SBC)&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="J107 P5V_SBC.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145011iA7B82FF046BCC257/image-size/large?v=v2&amp;amp;px=999" role="button" title="J107 P5V_SBC.jpg" alt="J107 P5V_SBC.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;J107 P5V_SBC.jpg&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;If you don't want to use external CAN transceiver, then you can connect CAN bus at J13.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CAN Physical Layer.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145012i34FE0FCD0607EE41/image-size/large?v=v2&amp;amp;px=999" role="button" title="CAN Physical Layer.jpg" alt="CAN Physical Layer.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;CAN Physical Layer.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 02:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-CAN-transceiver-with-NXP-example-model/m-p/1278550#M10906</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-05-19T02:36:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB CAN transceiver with NXP example model</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-CAN-transceiver-with-NXP-example-model/m-p/1279042#M10916</link>
      <description>&lt;P&gt;Solved, by taping some iffy CAN cable connections together.&lt;LI-EMOJI id="lia_fearful-face" title=":fearful_face:"&gt;&lt;/LI-EMOJI&gt; &amp;nbsp;I'm going to mark your answer,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57959"&gt;@Robin_Shen&lt;/a&gt;, as the correct one, however, so people can find the helpful info.&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 14:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-CAN-transceiver-with-NXP-example-model/m-p/1279042#M10916</guid>
      <dc:creator>neffnan</dc:creator>
      <dc:date>2021-05-19T14:26:40Z</dc:date>
    </item>
  </channel>
</rss>