<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K118 EEPROM emulation programming in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K118-EEPROM-emulation-programming/m-p/1278908#M10911</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Im using the S32K118 with winIDEA and want to use the EEPROM emulation. This is a completely new device for me.&lt;/P&gt;&lt;P&gt;Based on my understanding, when EEPROM emulation is enabled (EERDY=1), I should have no problem programming the addresses form 0x1400'0000 on.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wanted to do this via regular bus access but it does not work for me.&amp;nbsp;When writing 8 bytes, only lower 4 bytes are programmed. When writing 16 bytes, only first and third 4 byte chunks are programmed. Does this sound familiar by any chance?&lt;/P&gt;&lt;P&gt;I explored the option of getting this programmed with flash API but did not find a way since I can only use 3 bytes of address.&lt;/P&gt;&lt;P&gt;How can I make sure that EEPROM programming will work as expected?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;</description>
    <pubDate>Wed, 19 May 2021 10:27:02 GMT</pubDate>
    <dc:creator>RobertKalem</dc:creator>
    <dc:date>2021-05-19T10:27:02Z</dc:date>
    <item>
      <title>S32K118 EEPROM emulation programming</title>
      <link>https://community.nxp.com/t5/S32K/S32K118-EEPROM-emulation-programming/m-p/1278908#M10911</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Im using the S32K118 with winIDEA and want to use the EEPROM emulation. This is a completely new device for me.&lt;/P&gt;&lt;P&gt;Based on my understanding, when EEPROM emulation is enabled (EERDY=1), I should have no problem programming the addresses form 0x1400'0000 on.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wanted to do this via regular bus access but it does not work for me.&amp;nbsp;When writing 8 bytes, only lower 4 bytes are programmed. When writing 16 bytes, only first and third 4 byte chunks are programmed. Does this sound familiar by any chance?&lt;/P&gt;&lt;P&gt;I explored the option of getting this programmed with flash API but did not find a way since I can only use 3 bytes of address.&lt;/P&gt;&lt;P&gt;How can I make sure that EEPROM programming will work as expected?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 10:27:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118-EEPROM-emulation-programming/m-p/1278908#M10911</guid>
      <dc:creator>RobertKalem</dc:creator>
      <dc:date>2021-05-19T10:27:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K118 EEPROM emulation programming</title>
      <link>https://community.nxp.com/t5/S32K/S32K118-EEPROM-emulation-programming/m-p/1279057#M10917</link>
      <description>&lt;P&gt;Hi Robert,&lt;/P&gt;
&lt;P&gt;The EEPROM can be written in 8bit, 16bit or 32bit words, but each write clears the CCIF flag, and the program must wait until the flag is set again.&lt;/P&gt;
&lt;P&gt;For more information, please refer to AN11983 Using the S32K1xx EEPROM Functionality&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11983.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com/docs/en/application-note/AN11983.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 14:45:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118-EEPROM-emulation-programming/m-p/1279057#M10917</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-05-19T14:45:28Z</dc:date>
    </item>
  </channel>
</rss>