<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using one TRGMUX source for multiple target module? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Using-one-TRGMUX-source-for-multiple-target-module/m-p/1275811#M10865</link>
    <description>&lt;P&gt;Hi, I believe it should works. Configuration is not mutually exclusive, so could be able to assign TRGMUX input to multiple outputs.&lt;/P&gt;</description>
    <pubDate>Wed, 12 May 2021 17:09:53 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2021-05-12T17:09:53Z</dc:date>
    <item>
      <title>Using one TRGMUX source for multiple target module?</title>
      <link>https://community.nxp.com/t5/S32K/Using-one-TRGMUX-source-for-multiple-target-module/m-p/1273948#M10821</link>
      <description>&lt;P&gt;Is that possible to use one TRGMUX source&amp;nbsp;for multiple target modules in S32K14x?&amp;nbsp;&lt;/P&gt;&lt;P&gt;e.g.,&amp;nbsp;FTM0_INIT_TRIG to (DMA_CH0, ADC0_ADHWT,&amp;nbsp;LPUART0_TRG and&amp;nbsp;LPSPI0_TRG)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 08 May 2021 04:07:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-one-TRGMUX-source-for-multiple-target-module/m-p/1273948#M10821</guid>
      <dc:creator>JeorgeB</dc:creator>
      <dc:date>2021-05-08T04:07:01Z</dc:date>
    </item>
    <item>
      <title>Re: Using one TRGMUX source for multiple target module?</title>
      <link>https://community.nxp.com/t5/S32K/Using-one-TRGMUX-source-for-multiple-target-module/m-p/1275811#M10865</link>
      <description>&lt;P&gt;Hi, I believe it should works. Configuration is not mutually exclusive, so could be able to assign TRGMUX input to multiple outputs.&lt;/P&gt;</description>
      <pubDate>Wed, 12 May 2021 17:09:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-one-TRGMUX-source-for-multiple-target-module/m-p/1275811#M10865</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-05-12T17:09:53Z</dc:date>
    </item>
  </channel>
</rss>