<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32k148 First Block Flash Write is not happening.</title>
    <link>https://community.nxp.com/t5/S32K/S32k148-First-Block-Flash-Write-is-not-happening/m-p/1275332#M10849</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Problem Case&amp;nbsp; :&lt;BR /&gt;&lt;BR /&gt;I am using the s32k148 board, and in that first 512 kb of pFlash Block, I am using for the Bootloader and the Application code. i.e first 256kb I put the bootloader and in the next 256 kb I put the application.&lt;BR /&gt;&lt;BR /&gt;But now what I am trying to do is I want to write the new Application receiving via CAN in the Application part(Second 256 Kb part).&lt;BR /&gt;so for that, i am able to erase the Application Memory by entering in the Bootloader and by using Flash Erase.&lt;BR /&gt;but now the current problem is with I am able to receive the frames over CAN but not able to write at the memory location.&lt;BR /&gt;&lt;BR /&gt;Working Case :&lt;BR /&gt;&lt;BR /&gt;But when I put the Bootloader in the first 512 kb block, and the application in the second 512 kb block, then I am able to write the complete new received application over CAN in the Second Block.&lt;BR /&gt;so now the problem as I mention in the above case, when I am trying to do it in the single 512 kb Block then it's creating the writing problem.&lt;BR /&gt;&lt;BR /&gt;Kindly help me with this I am new to this kind of stuff.&lt;BR /&gt;&lt;BR /&gt;Thanks in Advance,&lt;BR /&gt;Rohit&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 12 May 2021 04:46:19 GMT</pubDate>
    <dc:creator>rohit_alate</dc:creator>
    <dc:date>2021-05-12T04:46:19Z</dc:date>
    <item>
      <title>S32k148 First Block Flash Write is not happening.</title>
      <link>https://community.nxp.com/t5/S32K/S32k148-First-Block-Flash-Write-is-not-happening/m-p/1275332#M10849</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Problem Case&amp;nbsp; :&lt;BR /&gt;&lt;BR /&gt;I am using the s32k148 board, and in that first 512 kb of pFlash Block, I am using for the Bootloader and the Application code. i.e first 256kb I put the bootloader and in the next 256 kb I put the application.&lt;BR /&gt;&lt;BR /&gt;But now what I am trying to do is I want to write the new Application receiving via CAN in the Application part(Second 256 Kb part).&lt;BR /&gt;so for that, i am able to erase the Application Memory by entering in the Bootloader and by using Flash Erase.&lt;BR /&gt;but now the current problem is with I am able to receive the frames over CAN but not able to write at the memory location.&lt;BR /&gt;&lt;BR /&gt;Working Case :&lt;BR /&gt;&lt;BR /&gt;But when I put the Bootloader in the first 512 kb block, and the application in the second 512 kb block, then I am able to write the complete new received application over CAN in the Second Block.&lt;BR /&gt;so now the problem as I mention in the above case, when I am trying to do it in the single 512 kb Block then it's creating the writing problem.&lt;BR /&gt;&lt;BR /&gt;Kindly help me with this I am new to this kind of stuff.&lt;BR /&gt;&lt;BR /&gt;Thanks in Advance,&lt;BR /&gt;Rohit&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 12 May 2021 04:46:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k148-First-Block-Flash-Write-is-not-happening/m-p/1275332#M10849</guid>
      <dc:creator>rohit_alate</dc:creator>
      <dc:date>2021-05-12T04:46:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32k148 First Block Flash Write is not happening.</title>
      <link>https://community.nxp.com/t5/S32K/S32k148-First-Block-Flash-Write-is-not-happening/m-p/1275446#M10858</link>
      <description>&lt;P&gt;Hello Rohit,&lt;/P&gt;
&lt;P&gt;It is not allowed to program/erase one block of PFlash (512KB) and read it (execute code from it) at the same time.&lt;/P&gt;
&lt;P&gt;All allowed simultaneous operations are shown in this table:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1620805162976.png" style="width: 546px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/144522i703B78BF8D037DCF/image-dimensions/546x563?v=v2" width="546" height="563" role="button" title="danielmartynek_0-1620805162976.png" alt="danielmartynek_0-1620805162976.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 May 2021 07:40:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k148-First-Block-Flash-Write-is-not-happening/m-p/1275446#M10858</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-05-12T07:40:03Z</dc:date>
    </item>
  </channel>
</rss>