<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Tolerance of LPIT CVAL (Current timer value)</title>
    <link>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1273632#M10812</link>
    <description>&lt;P&gt;If the LPIT’s bus interface clock and peripheral functional clock are derived from the same clock source, it can significantly reduce the problem. However, it's not 100% solution. Still the triple vote should be used. &lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Fri, 07 May 2021 10:01:09 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2021-05-07T10:01:09Z</dc:date>
    <item>
      <title>Tolerance of LPIT CVAL (Current timer value)</title>
      <link>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1273291#M10801</link>
      <description>&lt;P&gt;Regarding the CVAL (Current timer value) of NXP S32K144 LPIT, TRM states that "may not return the true value during operation"&lt;BR /&gt;However, could you clarify the tolerance of the values returned during LPIT running?&lt;/P&gt;&lt;P&gt;The lower bits of CVAL are truncated according to the required timer accuracy, so if the tolerance is within the truncated range, it can be used as the Current timer value.&lt;/P&gt;</description>
      <pubDate>Fri, 07 May 2021 00:01:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1273291#M10801</guid>
      <dc:creator>Hozumi</dc:creator>
      <dc:date>2021-05-07T00:01:12Z</dc:date>
    </item>
    <item>
      <title>Re: Tolerance of LPIT CVAL (Current timer value)</title>
      <link>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1273294#M10802</link>
      <description>&lt;P&gt;On the otherhand, TRM (Rev. 12.1, 02/2020) states that "At any time, the current value of the timer for any channel can be read by reading the corresponding channel's CVALn register. The M_CEN bit must be '1' when doing so." in 48.5.2 page1549.&lt;/P&gt;&lt;P&gt;What are the conditions under which the LPIT CVAL does not return the correct value?&lt;/P&gt;</description>
      <pubDate>Fri, 07 May 2021 00:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1273294#M10802</guid>
      <dc:creator>Hozumi</dc:creator>
      <dc:date>2021-05-07T00:04:23Z</dc:date>
    </item>
    <item>
      <title>Re: Tolerance of LPIT CVAL (Current timer value)</title>
      <link>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1273507#M10807</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;This weakness is caused by limited functionality on the internal synchronization gasket between LPIT’s bus interface block and peripheral functional clock. &lt;BR /&gt;It’s not possible to provide max expected difference between the reads because it depends on the particular bit that hasn’t yet transitioned to the correct value. &lt;BR /&gt;To identify potentially wrong read of the CVAL, it’s recommended to use triple vote method. &lt;BR /&gt;Regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 07 May 2021 07:58:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1273507#M10807</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-05-07T07:58:20Z</dc:date>
    </item>
    <item>
      <title>Re: Tolerance of LPIT CVAL (Current timer value)</title>
      <link>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1273547#M10809</link>
      <description>&lt;P&gt;Hi Lukas,&lt;/P&gt;&lt;P&gt;Depending on the relationship between the bus clock and the LPIT's count clock, can we read CVAL correctly?&lt;BR /&gt;For example, bus clock = LPIT's count clock.&lt;/P&gt;</description>
      <pubDate>Fri, 07 May 2021 08:28:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1273547#M10809</guid>
      <dc:creator>Hozumi</dc:creator>
      <dc:date>2021-05-07T08:28:27Z</dc:date>
    </item>
    <item>
      <title>Re: Tolerance of LPIT CVAL (Current timer value)</title>
      <link>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1273632#M10812</link>
      <description>&lt;P&gt;If the LPIT’s bus interface clock and peripheral functional clock are derived from the same clock source, it can significantly reduce the problem. However, it's not 100% solution. Still the triple vote should be used. &lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 07 May 2021 10:01:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1273632#M10812</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-05-07T10:01:09Z</dc:date>
    </item>
    <item>
      <title>Re: Tolerance of LPIT CVAL (Current timer value)</title>
      <link>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1276105#M10866</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37795"&gt;@lukaszadrapa&lt;/a&gt;, could you please introduce "&lt;SPAN&gt;triple vote method&lt;/SPAN&gt;" in detail ? Is it&amp;nbsp; a 100% solution ?&lt;/P&gt;</description>
      <pubDate>Thu, 13 May 2021 02:54:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1276105#M10866</guid>
      <dc:creator>vienpeng</dc:creator>
      <dc:date>2021-05-13T02:54:03Z</dc:date>
    </item>
    <item>
      <title>Re: Tolerance of LPIT CVAL (Current timer value)</title>
      <link>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1276471#M10877</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;triple vote method means that you perform three consecutive reads and then evaluate the result. If there's uneven value, discard it.&lt;/P&gt;
&lt;P&gt;The reads should be done as fast as possible. If it is done by CPU, use critical section, so no interrupt is triggered. Another option is to use DMA.&lt;/P&gt;
&lt;P&gt;I got information that the possibility to read wrong value is higher if ratio between peripheral clock and bus clock is lower. If the ratio is 1/24, at least, it can still occur but probability is smaller and triple vote will eliminate the problem. Or, as already mentioned, use the same clock source (but triple vote is also needed).&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 May 2021 15:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1276471#M10877</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-05-13T15:29:41Z</dc:date>
    </item>
    <item>
      <title>Re: Tolerance of LPIT CVAL (Current timer value)</title>
      <link>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1298824#M11211</link>
      <description>&lt;P&gt;Hi, Lukas&lt;/P&gt;&lt;P&gt;About your comment "possibility to read wrong value is higher if ratio between peripheral clock and bus clock is lower"&lt;/P&gt;&lt;P&gt;Please tell me why this problem occur ?&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jun 2021 04:03:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1298824#M11211</guid>
      <dc:creator>Hirofumi</dc:creator>
      <dc:date>2021-06-28T04:03:13Z</dc:date>
    </item>
    <item>
      <title>Re: Tolerance of LPIT CVAL (Current timer value)</title>
      <link>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1469268#M15796</link>
      <description>&lt;P&gt;Hi Lukas,&lt;/P&gt;&lt;P&gt;Regarding the reading of the CVAL of LPIT Driver, apart from reading in the ISR section which is already mentioned as the workaround for the errata the triple vote method is suggested to get the correct CVAL values. So, is this triple vote also can be added to the Errata workaround as an alternate solution for the CVAL Errata.&lt;/P&gt;&lt;P&gt;Please respond to the above query as soon as possible by tomorrow as it is an urgent need for the project.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;</description>
      <pubDate>Mon, 06 Jun 2022 09:53:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1469268#M15796</guid>
      <dc:creator>parth_rastogi10</dc:creator>
      <dc:date>2022-06-06T09:53:45Z</dc:date>
    </item>
    <item>
      <title>Re: Tolerance of LPIT CVAL (Current timer value)</title>
      <link>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1469973#M15828</link>
      <description>&lt;P&gt;Hi Lukas,&lt;/P&gt;&lt;P&gt;Can you please respond to the query that I posted for the workaround for reading CVAL.&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37795"&gt;@lukaszadrapa&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jun 2022 11:54:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tolerance-of-LPIT-CVAL-Current-timer-value/m-p/1469973#M15828</guid>
      <dc:creator>parth_rastogi10</dc:creator>
      <dc:date>2022-06-07T11:54:51Z</dc:date>
    </item>
  </channel>
</rss>