<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K144 FTM</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-FTM/m-p/1269636#M10714</link>
    <description>&lt;P&gt;i see the simple example use FTM0 CH0 as output compare,use FTM0 CH1 as edge-aligned PWM ,use FTM CH6 as input capture,by setting the register directly. i want use the RTM 3.0 to achieve the same goal.but i failed!I Can't set flexTimer_ic component's device and the ftm_oc component's device as FTM0 the same time.also i set different channel.&lt;/P&gt;&lt;P&gt;promblem is&amp;nbsp;Peripheral is already used .&lt;/P&gt;&lt;P&gt;how should i do?thanks.@NXP&lt;/P&gt;</description>
    <pubDate>Wed, 28 Apr 2021 12:13:47 GMT</pubDate>
    <dc:creator>julywu</dc:creator>
    <dc:date>2021-04-28T12:13:47Z</dc:date>
    <item>
      <title>S32K144 FTM</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FTM/m-p/1269636#M10714</link>
      <description>&lt;P&gt;i see the simple example use FTM0 CH0 as output compare,use FTM0 CH1 as edge-aligned PWM ,use FTM CH6 as input capture,by setting the register directly. i want use the RTM 3.0 to achieve the same goal.but i failed!I Can't set flexTimer_ic component's device and the ftm_oc component's device as FTM0 the same time.also i set different channel.&lt;/P&gt;&lt;P&gt;promblem is&amp;nbsp;Peripheral is already used .&lt;/P&gt;&lt;P&gt;how should i do?thanks.@NXP&lt;/P&gt;</description>
      <pubDate>Wed, 28 Apr 2021 12:13:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FTM/m-p/1269636#M10714</guid>
      <dc:creator>julywu</dc:creator>
      <dc:date>2021-04-28T12:13:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 FTM</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FTM/m-p/1272568#M10791</link>
      <description>&lt;P&gt;Hi&amp;nbsp;julywu,&lt;/P&gt;
&lt;P&gt;FTM can be used with different settings configuration in the same FTM different channel. The problem here is that the SDK driver &lt;STRONG&gt;ic&lt;/STRONG&gt; and &lt;STRONG&gt;oc&lt;/STRONG&gt; were made independently, so they cannot coexist with the same FTM module. Ideally speaking, the driver should be able to set a component &lt;STRONG&gt;ic&lt;/STRONG&gt; in one channel, and set a component &lt;STRONG&gt;oc&lt;/STRONG&gt; with another channel, and be able to identify that it is not the same channel.&lt;/P&gt;
&lt;P&gt;I will share this feedback with the SW team to integrate this functionality into the new RTD for the K1 project.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Sorry for the inconvenience we bring you!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 06 May 2021 02:31:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FTM/m-p/1272568#M10791</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-05-06T02:31:53Z</dc:date>
    </item>
  </channel>
</rss>