<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ECC Flash Error in S32K</title>
    <link>https://community.nxp.com/t5/S32K/ECC-Flash-Error/m-p/1269603#M10708</link>
    <description>&lt;P&gt;When will the double bit ECC error for Flash is set?. Will it set if there is a checksum fault in flash?.&lt;/P&gt;</description>
    <pubDate>Wed, 28 Apr 2021 10:38:17 GMT</pubDate>
    <dc:creator>rijil_kp</dc:creator>
    <dc:date>2021-04-28T10:38:17Z</dc:date>
    <item>
      <title>ECC Flash Error</title>
      <link>https://community.nxp.com/t5/S32K/ECC-Flash-Error/m-p/1268151#M10671</link>
      <description>&lt;P&gt;How to generate an interrupt notification upon the report of an ECC flash error,?.&lt;/P&gt;&lt;P&gt;Is there any configurations available in EB Tresos for this?.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Apr 2021 12:12:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ECC-Flash-Error/m-p/1268151#M10671</guid>
      <dc:creator>rijil_kp</dc:creator>
      <dc:date>2021-04-26T12:12:00Z</dc:date>
    </item>
    <item>
      <title>Re: ECC Flash Error</title>
      <link>https://community.nxp.com/t5/S32K/ECC-Flash-Error/m-p/1268644#M10680</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/149991"&gt;@rijil_kp&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Any single-bit ECC errors are automatically corrected, and any double-bit ECC errors are reflected onto FERSTAT[DFDIF] flag at the read access from Data Flash or Program Flash. This double-bit ECC error is reported by bus fault/hard fault handler. There isn't any configuration for report the ECC flash error in EB Tresos, unfortunately.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Nam&lt;/P&gt;</description>
      <pubDate>Tue, 27 Apr 2021 07:19:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ECC-Flash-Error/m-p/1268644#M10680</guid>
      <dc:creator>namnguyenviet</dc:creator>
      <dc:date>2021-04-27T07:19:30Z</dc:date>
    </item>
    <item>
      <title>Re: ECC Flash Error</title>
      <link>https://community.nxp.com/t5/S32K/ECC-Flash-Error/m-p/1269603#M10708</link>
      <description>&lt;P&gt;When will the double bit ECC error for Flash is set?. Will it set if there is a checksum fault in flash?.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Apr 2021 10:38:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ECC-Flash-Error/m-p/1269603#M10708</guid>
      <dc:creator>rijil_kp</dc:creator>
      <dc:date>2021-04-28T10:38:17Z</dc:date>
    </item>
    <item>
      <title>Re: ECC Flash Error</title>
      <link>https://community.nxp.com/t5/S32K/ECC-Flash-Error/m-p/1269624#M10712</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can refer to here:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K-ECC-error/m-p/878734" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K-ECC-error/m-p/878734&lt;/A&gt;&amp;nbsp;and here:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12522.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12522.pdf&lt;/A&gt;&amp;nbsp;Basically, the ECC will be reported when the FLS read failed while checking the checksum value.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Apr 2021 11:50:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ECC-Flash-Error/m-p/1269624#M10712</guid>
      <dc:creator>namnguyenviet</dc:creator>
      <dc:date>2021-04-28T11:50:51Z</dc:date>
    </item>
  </channel>
</rss>