<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Edge interrupt</title>
    <link>https://community.nxp.com/t5/S32K/Edge-interrupt/m-p/686269#M1068</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Power_Manager SDK Example uses a port interrupt on PTC13 to wake up from a sleep mode. This is the only example we have, unfortunately.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Jun 2017 07:44:55 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2017-06-15T07:44:55Z</dc:date>
    <item>
      <title>Edge interrupt</title>
      <link>https://community.nxp.com/t5/S32K/Edge-interrupt/m-p/686268#M1067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;Do we have any examples of interruption by a rising edge?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2017 14:49:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Edge-interrupt/m-p/686268#M1067</guid>
      <dc:creator>lohrsistemas</dc:creator>
      <dc:date>2017-06-14T14:49:28Z</dc:date>
    </item>
    <item>
      <title>Re: Edge interrupt</title>
      <link>https://community.nxp.com/t5/S32K/Edge-interrupt/m-p/686269#M1068</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Power_Manager SDK Example uses a port interrupt on PTC13 to wake up from a sleep mode. This is the only example we have, unfortunately.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jun 2017 07:44:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Edge-interrupt/m-p/686269#M1068</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-06-15T07:44:55Z</dc:date>
    </item>
    <item>
      <title>Re: Edge interrupt</title>
      <link>https://community.nxp.com/t5/S32K/Edge-interrupt/m-p/686270#M1069</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/lohrsistemas"&gt;lohrsistemas&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case you have Matlab and you are familiar with model based design - then you can create your own examples very easily. Even if you do not want to use it for final product development it can be a good resource to generate C-code examples since it is based on the same S32K SDK release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a snippet of that you can do with it:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20904i8D5DD92D1A06804A/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20951i5078B69BDD0B6B6E/image-size/large?v=v2&amp;amp;px=999" title="2.JPG" alt="2.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If interested you can get if from here:&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-334170"&gt;https://community.nxp.com/docs/DOC-334170&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;*Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jun 2017 08:49:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Edge-interrupt/m-p/686270#M1069</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2017-06-15T08:49:56Z</dc:date>
    </item>
  </channel>
</rss>