<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32R294 SPE in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32R294-SPE/m-p/1265776#M10625</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;As reference manual express:&lt;/P&gt;
&lt;P&gt;SPE accelerates operations via the use of short vectors (two, four, or eight elements) within 64-bit&lt;BR /&gt;GPRs and the use of Single Instruction Multiple Data (SIMD) operations. SPE 2.1 also includes an accumulator register to allow&lt;BR /&gt;for certain back-to-back operations without loop unrolling.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
    <pubDate>Wed, 21 Apr 2021 10:17:01 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2021-04-21T10:17:01Z</dc:date>
    <item>
      <title>S32R294 SPE</title>
      <link>https://community.nxp.com/t5/S32K/S32R294-SPE/m-p/1265009#M10610</link>
      <description>&lt;P&gt;SPE does not look like much faster than C,why?&lt;/P&gt;&lt;P&gt;this is my code with C and SPE.&lt;/P&gt;&lt;P&gt;/******code with C*******/&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="code With C" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/142755iD38C9F5327C3D5CA/image-size/large?v=v2&amp;amp;px=999" role="button" title="c.PNG" alt="code With C" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;code With C&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;/******code with SPE*******/&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="code With SPE" style="width: 951px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/142756iB856ABC437A4F813/image-size/large?v=v2&amp;amp;px=999" role="button" title="spe.png" alt="code With SPE" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;code With SPE&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 09:11:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32R294-SPE/m-p/1265009#M10610</guid>
      <dc:creator>Yanyang_smile</dc:creator>
      <dc:date>2021-04-20T09:11:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32R294 SPE</title>
      <link>https://community.nxp.com/t5/S32K/S32R294-SPE/m-p/1265776#M10625</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;As reference manual express:&lt;/P&gt;
&lt;P&gt;SPE accelerates operations via the use of short vectors (two, four, or eight elements) within 64-bit&lt;BR /&gt;GPRs and the use of Single Instruction Multiple Data (SIMD) operations. SPE 2.1 also includes an accumulator register to allow&lt;BR /&gt;for certain back-to-back operations without loop unrolling.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Wed, 21 Apr 2021 10:17:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32R294-SPE/m-p/1265776#M10625</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2021-04-21T10:17:01Z</dc:date>
    </item>
  </channel>
</rss>