<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Help receiving and writing data with unified bootloader framework for S32K116 with LIN in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Help-receiving-and-writing-data-with-unified-bootloader/m-p/1263049#M10575</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;not further docs is available, just 2 guides you already have, i think, and demo projects in unified bootloader package.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Thu, 15 Apr 2021 20:19:57 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2021-04-15T20:19:57Z</dc:date>
    <item>
      <title>Help receiving and writing data with unified bootloader framework for S32K116 with LIN</title>
      <link>https://community.nxp.com/t5/S32K/Help-receiving-and-writing-data-with-unified-bootloader/m-p/1256777#M10441</link>
      <description>&lt;P&gt;I’m trying to use the unified bootloader framework with LIN for writing a new srec file on the microcontroller.&lt;/P&gt;&lt;P&gt;But I’m struggling a little bit with understanding the main format or process that is required to read &amp;amp; write data successfully since the code seems a little bit tangled up.&lt;/P&gt;&lt;P&gt;Is there further documentation to understand the code, or could you please give me a brief explanation/description of how the data should be received and sent to write a new srec file on the microcontroller?&lt;/P&gt;&lt;P&gt;For example, on the previous bootloader the first 2 bits of the received data should be (0x00, 0x01) in order to enter to the sessionStatus as SS_CONNECTED.&lt;/P&gt;&lt;P&gt;I would like to know this kind of characteristics for this new unified bootloader. Or for example, where/how is "g_pstFlashOptInfo-&amp;gt;FLASH_Program" set? ( when I look into its references there is no "set" reference).&lt;/P&gt;</description>
      <pubDate>Mon, 05 Apr 2021 17:55:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Help-receiving-and-writing-data-with-unified-bootloader/m-p/1256777#M10441</guid>
      <dc:creator>HayZam</dc:creator>
      <dc:date>2021-04-05T17:55:34Z</dc:date>
    </item>
    <item>
      <title>Re: Help receiving and writing data with unified bootloader framework for S32K116 with LIN</title>
      <link>https://community.nxp.com/t5/S32K/Help-receiving-and-writing-data-with-unified-bootloader/m-p/1263049#M10575</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;not further docs is available, just 2 guides you already have, i think, and demo projects in unified bootloader package.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 20:19:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Help-receiving-and-writing-data-with-unified-bootloader/m-p/1263049#M10575</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-04-15T20:19:57Z</dc:date>
    </item>
  </channel>
</rss>