<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K142 Custom Board Programming Issues in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K142-Custom-Board-Programming-Issues/m-p/1261337#M10541</link>
    <description>&lt;P&gt;Hi Lukas,&lt;/P&gt;&lt;P&gt;Sorry for the confusion but the RESET pin's measurements are there whether I connect the debugger or not. The microcontroller's Reset pin is always showing the described behavior when I connect it to power. Can you look into the possible causes of this?&lt;/P&gt;&lt;P&gt;I have also tried to program the microcontroller with J-Link using SWD but could not program it.&lt;/P&gt;</description>
    <pubDate>Tue, 13 Apr 2021 13:40:45 GMT</pubDate>
    <dc:creator>talha_uyar</dc:creator>
    <dc:date>2021-04-13T13:40:45Z</dc:date>
    <item>
      <title>S32K142 Custom Board Programming Issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K142-Custom-Board-Programming-Issues/m-p/1261202#M10536</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have designed a custom board for our S32K142. I am trying to program it using the OpenSDA on my S32K142 EVB. I have connected J14's Pin_2, Pin_4, Pin_10, and Pin_3 (SWD_DIO, SWD_CLK, RST_TGTMCU_B, and GND) to the custom board. Then, I have tried to flash something to the custom board but I have failed.&lt;/P&gt;&lt;P&gt;When I measure the RST_TGTMCU_B with an oscilloscope I see that it is not held low and instead oscillates between 2.5V and 0V (see attached image). I think the microcontroller is resetting itself but I don't know why. What could be the issue here? We have connected a 24 MHz XTAL to PTB6 and PTB7. Could this be the issue?&lt;/P&gt;&lt;P&gt;Thanks for all the help&lt;/P&gt;</description>
      <pubDate>Tue, 13 Apr 2021 10:30:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K142-Custom-Board-Programming-Issues/m-p/1261202#M10536</guid>
      <dc:creator>talha_uyar</dc:creator>
      <dc:date>2021-04-13T10:30:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32K142 Custom Board Programming Issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K142-Custom-Board-Programming-Issues/m-p/1261325#M10540</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I'm afraid this is not expected use-case. You are talking to two microcontrollers at the same time, so there could be a conflict between the signals. Better solution is to use debug probe like:&lt;/P&gt;
&lt;P&gt;&lt;A href="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320168&amp;amp;productTab=1" target="_blank"&gt;http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320168&amp;amp;productTab=1&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;or&lt;/P&gt;
&lt;P&gt;&lt;A href="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320143&amp;amp;productTab=1" target="_blank"&gt;http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320143&amp;amp;productTab=1&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Apr 2021 13:30:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K142-Custom-Board-Programming-Issues/m-p/1261325#M10540</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-04-13T13:30:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32K142 Custom Board Programming Issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K142-Custom-Board-Programming-Issues/m-p/1261337#M10541</link>
      <description>&lt;P&gt;Hi Lukas,&lt;/P&gt;&lt;P&gt;Sorry for the confusion but the RESET pin's measurements are there whether I connect the debugger or not. The microcontroller's Reset pin is always showing the described behavior when I connect it to power. Can you look into the possible causes of this?&lt;/P&gt;&lt;P&gt;I have also tried to program the microcontroller with J-Link using SWD but could not program it.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Apr 2021 13:40:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K142-Custom-Board-Programming-Issues/m-p/1261337#M10541</guid>
      <dc:creator>talha_uyar</dc:creator>
      <dc:date>2021-04-13T13:40:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32K142 Custom Board Programming Issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K142-Custom-Board-Programming-Issues/m-p/1262067#M10557</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;some useful hints for recovery can be found in this thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K142-EVB-board-bricks/m-p/1157622" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K142-EVB-board-bricks/m-p/1157622&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Do you mean you replaced original 8MHz crystal? It should be no problem, the frequency can be 4 - 40MHz.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 13:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K142-Custom-Board-Programming-Issues/m-p/1262067#M10557</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-04-14T13:43:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K142 Custom Board Programming Issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K142-Custom-Board-Programming-Issues/m-p/1262510#M10566</link>
      <description>&lt;P&gt;Hi Lukas,&lt;/P&gt;&lt;P&gt;I have solved my problem and it was rather simple. We had a capacitor connected to the reset pin and the S32K142 was resetting itself since it had no code. This was resulting in the behavior I have posted here. I removed the capacitor and used JLink to flash. I also added the line "monitor reset" to the debugger's startup tab in S32 DS as described &lt;A title="Reset pin stays low on S32K144" href="https://community.nxp.com/t5/S32K/Reset-pin-stays-low-on-S32K144/m-p/714520/thread-id/1581" target="_self"&gt;here&lt;/A&gt;&amp;nbsp;. The JLink successfully flashed the S32K142.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;M. Talha Uyar&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 05:58:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K142-Custom-Board-Programming-Issues/m-p/1262510#M10566</guid>
      <dc:creator>talha_uyar</dc:creator>
      <dc:date>2021-04-15T05:58:59Z</dc:date>
    </item>
  </channel>
</rss>