<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Program file does not exist</title>
    <link>https://community.nxp.com/t5/S32K/Program-file-does-not-exist/m-p/1258842#M10483</link>
    <description>&lt;P&gt;Solved!&lt;/P&gt;&lt;P&gt;Target .elf file was not specified:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture3.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/141685i07093DD3186F1D79/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture3.PNG" alt="Capture3.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 08 Apr 2021 11:19:02 GMT</pubDate>
    <dc:creator>Nando</dc:creator>
    <dc:date>2021-04-08T11:19:02Z</dc:date>
    <item>
      <title>Program file does not exist</title>
      <link>https://community.nxp.com/t5/S32K/Program-file-does-not-exist/m-p/1258580#M10480</link>
      <description>&lt;P&gt;I have seen this topic came up several times but I have not found a solution that works for me.&lt;BR /&gt;So: I am taking over a project. It used to work with a colleague and it also works with another colleague who is also taking over a part. So the problem is with my installation or setup.&lt;BR /&gt;It is a version of the S32K144_PT200_EXAMPLE. It builds fine but I cannot debug it. I also could not communicate with the board using Freemaster.&lt;BR /&gt;I have two debug options:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/141615iFBD59917B7EC7ABC/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I was told to use the PE micro one and set it up as above. However cross_prefix and cross_suffix are defined as:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture2.PNG" style="width: 696px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/141617i67BD2462BA0D4F01/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture2.PNG" alt="Capture2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and I have a gdb on that path:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture3.PNG" style="width: 799px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/141620iA2DCE34E488DFAAD/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture3.PNG" alt="Capture3.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So what does that error mean? Program file does not exist? Maybe it cannot find the compile outputs - the .elf file or something? Maybe the search path is wrong, but where do I set that?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Thu, 08 Apr 2021 06:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Program-file-does-not-exist/m-p/1258580#M10480</guid>
      <dc:creator>Nando</dc:creator>
      <dc:date>2021-04-08T06:16:01Z</dc:date>
    </item>
    <item>
      <title>Re: Program file does not exist</title>
      <link>https://community.nxp.com/t5/S32K/Program-file-does-not-exist/m-p/1258842#M10483</link>
      <description>&lt;P&gt;Solved!&lt;/P&gt;&lt;P&gt;Target .elf file was not specified:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture3.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/141685i07093DD3186F1D79/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture3.PNG" alt="Capture3.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Apr 2021 11:19:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Program-file-does-not-exist/m-p/1258842#M10483</guid>
      <dc:creator>Nando</dc:creator>
      <dc:date>2021-04-08T11:19:02Z</dc:date>
    </item>
  </channel>
</rss>