<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K116 EVB problem pwm using in function in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K116-EVB-problem-pwm-using-in-function/m-p/1256954#M10445</link>
    <description>&lt;P&gt;Hello, I'am using S32K116 evb. I want to use pwm driver but if i use this function in another function and i call this function in while() there is a problem. If i use ftm pwm driver in while loop, there is not problem. I add picture about this problem. Why is there this problem?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 06 Apr 2021 05:00:47 GMT</pubDate>
    <dc:creator>mfatihkoseoglu</dc:creator>
    <dc:date>2021-04-06T05:00:47Z</dc:date>
    <item>
      <title>S32K116 EVB problem pwm using in function</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-EVB-problem-pwm-using-in-function/m-p/1256954#M10445</link>
      <description>&lt;P&gt;Hello, I'am using S32K116 evb. I want to use pwm driver but if i use this function in another function and i call this function in while() there is a problem. If i use ftm pwm driver in while loop, there is not problem. I add picture about this problem. Why is there this problem?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Apr 2021 05:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-EVB-problem-pwm-using-in-function/m-p/1256954#M10445</guid>
      <dc:creator>mfatihkoseoglu</dc:creator>
      <dc:date>2021-04-06T05:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K116 EVB problem pwm using in function</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-EVB-problem-pwm-using-in-function/m-p/1260746#M10523</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;Hope you are well.&lt;BR /&gt;The status of the function is read through a variable type &lt;EM&gt;status_t&lt;/EM&gt;. Adding a small delay when the function is called could solve the problem.&lt;BR /&gt;Besides moving the methods of the function to a while are doing another change to the function. A more detailed description of the function might help.&lt;/P&gt;
&lt;P&gt;Let me know if this solves the problem, if you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 12 Apr 2021 20:18:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-EVB-problem-pwm-using-in-function/m-p/1260746#M10523</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-04-12T20:18:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K116 EVB problem pwm using in function</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-EVB-problem-pwm-using-in-function/m-p/1261049#M10530</link>
      <description>&lt;P&gt;Hello Omar,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks, I am fine and hope you too.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I add a delay and this func is work. But why? Why I use delay?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Apr 2021 07:19:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-EVB-problem-pwm-using-in-function/m-p/1261049#M10530</guid>
      <dc:creator>mfatihkoseoglu</dc:creator>
      <dc:date>2021-04-13T07:19:13Z</dc:date>
    </item>
    <item>
      <title>Re: S32K116 EVB problem pwm using in function</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-EVB-problem-pwm-using-in-function/m-p/1267463#M10660</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;The registers you update in the FTM_DRV_UpdatePwmChannel() function need some cycles to be updated. You can consult it in detail in chapter 47.5.12.3 of the reference manual.&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Fri, 23 Apr 2021 19:25:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-EVB-problem-pwm-using-in-function/m-p/1267463#M10660</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-04-23T19:25:49Z</dc:date>
    </item>
  </channel>
</rss>