<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K144 CAN TX interrupt issue</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-CAN-TX-interrupt-issue/m-p/1256560#M10436</link>
    <description>Hello everyone, Good day! I have a S32K144 application facing a problem. While a CAN message is transmitted, the corresponding CAN_IMASK1 and CAN_IFLAG1 bit is set. but it can't generate TX interrupt. (it can generate RX interrupt while a CAN message is received) Could anyone tell me where is wrong? IDE: S32DS_ARM_v2018.R1 Compiler: IAR ANSI C/C++ Compiler V8.32.3.193/W32 for ARM SDK: S32SDK_S32K1xx_RTM_3.0.0</description>
    <pubDate>Mon, 05 Apr 2021 05:51:55 GMT</pubDate>
    <dc:creator>jianxun_liu</dc:creator>
    <dc:date>2021-04-05T05:51:55Z</dc:date>
    <item>
      <title>S32K144 CAN TX interrupt issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-CAN-TX-interrupt-issue/m-p/1256560#M10436</link>
      <description>Hello everyone, Good day! I have a S32K144 application facing a problem. While a CAN message is transmitted, the corresponding CAN_IMASK1 and CAN_IFLAG1 bit is set. but it can't generate TX interrupt. (it can generate RX interrupt while a CAN message is received) Could anyone tell me where is wrong? IDE: S32DS_ARM_v2018.R1 Compiler: IAR ANSI C/C++ Compiler V8.32.3.193/W32 for ARM SDK: S32SDK_S32K1xx_RTM_3.0.0</description>
      <pubDate>Mon, 05 Apr 2021 05:51:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-CAN-TX-interrupt-issue/m-p/1256560#M10436</guid>
      <dc:creator>jianxun_liu</dc:creator>
      <dc:date>2021-04-05T05:51:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 CAN TX interrupt issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-CAN-TX-interrupt-issue/m-p/1256962#M10446</link>
      <description>&lt;P&gt;after further analysis, I found not any message receiving can generate RX interrupt.&lt;/P&gt;&lt;P&gt;only messages in MB ID 0 ~ 15 can generate RX interrupt.&lt;/P&gt;&lt;P&gt;messages in MB ID 16~31 can't generate interrupt no matter TX or RX.&lt;/P&gt;&lt;P&gt;I don't know why&amp;nbsp;CAN0_ORed_16_31_MB_IRQHandler interrupt can't be generated.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Apr 2021 05:12:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-CAN-TX-interrupt-issue/m-p/1256962#M10446</guid>
      <dc:creator>jianxun_liu</dc:creator>
      <dc:date>2021-04-06T05:12:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 CAN TX interrupt issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-CAN-TX-interrupt-issue/m-p/1259491#M10492</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;did you modify max available MBs within FlexCAN component? By default 16 MBs are used.&lt;BR /&gt;I tried demo example within S32DS.ARM.2.2, SDK_RTM3.0.2 (but using GCC compiler), changed max MBs to 32 and used e.g MB 17 and 21 for TX resp. RX functions and &lt;SPAN&gt;CAN0_ORed_16_31_MB_IRQHandler&amp;nbsp;&lt;/SPAN&gt;was called normally as expected.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 09 Apr 2021 08:12:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-CAN-TX-interrupt-issue/m-p/1259491#M10492</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-04-09T08:12:01Z</dc:date>
    </item>
  </channel>
</rss>