<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K144 no access via debug interface</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1252035#M10314</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can simply reprogram (by any example code) flash or erase it via debugger or via application.&lt;/P&gt;
&lt;P&gt;Have in mind to not leave empty boot vector at address 0x0 or the device will be locked.&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
    <pubDate>Thu, 25 Mar 2021 09:42:41 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2021-03-25T09:42:41Z</dc:date>
    <item>
      <title>S32K144 no access via debug interface</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1249789#M10261</link>
      <description>&lt;P&gt;&lt;FONT size="2"&gt;Hello Together,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;i have some problems with a S32K144.&amp;nbsp;&lt;/FONT&gt;&lt;FONT size="2"&gt;I was able to debug and flash the device for quite some time.&lt;BR /&gt;&lt;/FONT&gt;&lt;FONT size="2"&gt;I have prgrammed the S32K144 from a seond controller via SWD but I must done somting wrong.&amp;nbsp;&lt;BR /&gt;&lt;/FONT&gt;&lt;FONT size="2"&gt;Now it is not more posibble to connect the prozessor with debug interface.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The content of console:&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Connecting to J-Link...&lt;BR /&gt;J-Link is connected.&lt;BR /&gt;Firmware: J-Link V10 compiled Jan 7 2019 14:00:10&lt;BR /&gt;Hardware: V10.10&lt;BR /&gt;S/N: 50111539&lt;BR /&gt;Feature(s): GDB&lt;BR /&gt;Checking target voltage...&lt;BR /&gt;Target voltage: 3.28 V&lt;BR /&gt;Listening on TCP/IP port 2331&lt;BR /&gt;Connecting to target...&lt;BR /&gt;J-Link found 1 JTAG device, Total IRLen = 4&lt;BR /&gt;JTAG ID: 0x1993D01D (Cortex-M4)&lt;BR /&gt;Connected to target&lt;BR /&gt;Waiting for GDB connection...Connected to 127.0.0.1&lt;BR /&gt;Reading all registers&lt;BR /&gt;Read 4 bytes @ address 0x00000000 (Data = 0x20007000)&lt;BR /&gt;Read 2 bytes @ address 0x00000000 (Data = 0x7000)&lt;BR /&gt;Received monitor command: speed 1000&lt;BR /&gt;Target interface speed set to 1000 kHz&lt;BR /&gt;Received monitor command: clrbp&lt;BR /&gt;Received monitor command: reset&lt;BR /&gt;Resetting target&lt;BR /&gt;Received monitor command: halt&lt;BR /&gt;Halting target CPU...&lt;BR /&gt;...Target halted (PC = 0x0000069C)&lt;BR /&gt;Received monitor command: regs&lt;BR /&gt;R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000&lt;BR /&gt;R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000&lt;BR /&gt;R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000&lt;BR /&gt;R12= 00000000, R13= 20007000, MSP= 20007000, PSP= 00000000&lt;BR /&gt;R14(LR) = FFFFFFFF, R15(PC) = 0000069C&lt;BR /&gt;XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000&lt;BR /&gt;CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00&lt;BR /&gt;Reading all registers&lt;BR /&gt;Read 4 bytes @ address 0x0000069C (Data = 0xF04FB672)&lt;BR /&gt;Read 2 bytes @ address 0x0000069C (Data = 0xB672)&lt;BR /&gt;Received monitor command: speed auto&lt;BR /&gt;Select auto target interface speed (4000 kHz)&lt;BR /&gt;Received monitor command: flash breakpoints 1&lt;BR /&gt;Flash breakpoints enabled&lt;BR /&gt;Received monitor command: semihosting enable&lt;BR /&gt;Semi-hosting enabled (Handle on BKPT)&lt;BR /&gt;Received monitor command: semihosting IOClient 1&lt;BR /&gt;Semihosting I/O set to TELNET Client&lt;BR /&gt;Read 4 bytes @ address 0x0000069C (Data = 0xF04FB672)&lt;BR /&gt;Read 2 bytes @ address 0x0000069C (Data = 0xB672)&lt;BR /&gt;Downloading 1024 bytes @ address 0x00000000 - Verified OK&lt;BR /&gt;Downloading 16 bytes @ address 0x00000400 - Verified OK&lt;BR /&gt;Downloading 220 bytes @ address 0x00000410 - Verified OK&lt;BR /&gt;Downloading 4 bytes @ address 0x00000500 - Verified OK&lt;BR /&gt;Downloading 44 bytes @ address 0x00000504 - Verified OK&lt;BR /&gt;Downloading 24 bytes @ address 0x000005C0 - Verified OK&lt;BR /&gt;Downloading 24 bytes @ address 0x000005E0 - Verified OK&lt;BR /&gt;Downloading 16152 bytes @ address 0x000005F8 - Verified OK&lt;BR /&gt;Downloading 16160 bytes @ address 0x00004510 - Verified OK&lt;BR /&gt;Downloading 15920 bytes @ address 0x00008430 - Verified OK&lt;BR /&gt;Downloading 16048 bytes @ address 0x0000C260 - Verified OK&lt;BR /&gt;Downloading 16304 bytes @ address 0x00010110 - Verified OK&lt;BR /&gt;Downloading 13168 bytes @ address 0x000140C0 - Verified OK&lt;BR /&gt;Downloading 4 bytes @ address 0x00017430 - Verified OK&lt;BR /&gt;Downloading 4 bytes @ address 0x00017434 - Verified OK&lt;BR /&gt;Downloading 1908 bytes @ address 0x00017438 - Verified OK&lt;BR /&gt;Downloading 8816 bytes @ address 0x00017BAC - Verified OK&lt;BR /&gt;Downloading 16368 bytes @ address 0x00019E20 - Verified OK&lt;BR /&gt;Downloading 16 bytes @ address 0x0001DE10 - Verified OK&lt;BR /&gt;Read 4 bytes @ address 0x0000069C (Data = 0xF04FB672)&lt;BR /&gt;Read 2 bytes @ address 0x0000069C (Data = 0xB672)&lt;BR /&gt;Read 2 bytes @ address 0x000030B2 (Data = 0xF002)&lt;BR /&gt;Read 2 bytes @ address 0x000030B2 (Data = 0xF002)&lt;BR /&gt;Received monitor command: clrbp&lt;BR /&gt;Received monitor command: reset&lt;BR /&gt;Comparing flash [....................] Done.&lt;BR /&gt;Erasing flash [....................] Done.&lt;BR /&gt;Verifying flash [....................] Done.&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;ERROR: Timeout while restoring target, RAMCode did not respond in time. (PC = 0x00000000, CPSR = 0x00000000, LR = 0x81000003)!&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;Failed to restore target. RAMCode never stops&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;Failed to erase sectors 8 @ address 0x00008000 (unspecified error)&lt;/FONT&gt;&lt;BR /&gt;Resetting target&lt;BR /&gt;Received monitor command: halt&lt;BR /&gt;Halting target CPU...&lt;BR /&gt;...Target halted (PC = 0x0000069C)&lt;BR /&gt;Read 2 bytes @ address 0x000030B2 (Data = 0xF002)&lt;BR /&gt;Read 2 bytes @ address 0x000030B2 (Data = 0xF002)&lt;BR /&gt;Read 2 bytes @ address 0x000030B2 (Data = 0xF002)&lt;BR /&gt;Received monitor command: regs&lt;BR /&gt;R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000&lt;BR /&gt;R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000&lt;BR /&gt;R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000&lt;BR /&gt;R12= 00000000, R13= 20007000, MSP= 20007000, PSP= 00000000&lt;BR /&gt;R14(LR) = FFFFFFFF, R15(PC) = 0000069C&lt;BR /&gt;XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000&lt;BR /&gt;CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00&lt;BR /&gt;Reading all registers&lt;BR /&gt;Read 4 bytes @ address 0x0000069C (Data = 0xF04FB672)&lt;BR /&gt;Read 2 bytes @ address 0x0000069C (Data = 0xB672)&lt;BR /&gt;Setting breakpoint @ address 0x000030B2, Size = 2, BPHandle = 0x0001&lt;BR /&gt;Starting target CPU...&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Lutz&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 15:58:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1249789#M10261</guid>
      <dc:creator>koehlerl</dc:creator>
      <dc:date>2021-03-22T15:58:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 no access via debug interface</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1250448#M10277</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Is it possible to attach to running target?&lt;/P&gt;
&lt;P&gt;Try some example code instead of the current one. It is possible that your project is rewriting RAM where is Segger code, etc...&lt;/P&gt;
&lt;P&gt;Could you try it with PEMicro?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Tue, 23 Mar 2021 12:51:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1250448#M10277</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2021-03-23T12:51:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 no access via debug interface</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1250587#M10283</link>
      <description>&lt;P&gt;It is possible to connet the target.&lt;/P&gt;&lt;P&gt;But it does not work.&lt;/P&gt;&lt;P&gt;There are wrong things in the memory?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Memory Windo.JPG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/140436i098EB3276247D299/image-size/large?v=v2&amp;amp;px=999" role="button" title="Memory Windo.JPG" alt="Memory Windo.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Memory Windo.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It is possible to damge or lock the prozessor with wrong flash programming.&lt;/P&gt;&lt;P&gt;BR Lutz&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Mar 2021 16:07:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1250587#M10283</guid>
      <dc:creator>koehlerl</dc:creator>
      <dc:date>2021-03-23T16:07:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 no access via debug interface</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1251166#M10296</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;It is possible to damage or lock the processor with wrong flash programming.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Sure that's possible. You can lock it by erasing the boot header.&lt;/P&gt;
&lt;P&gt;You also have lots of ECC errors in flash, which can cause a lot of issues. Looks like your programming wasn't finish or done properly.&lt;/P&gt;
&lt;P&gt;Is it possible to load any example code to the device?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Wed, 24 Mar 2021 10:54:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1251166#M10296</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2021-03-24T10:54:53Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 no access via debug interface</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1251213#M10298</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;yes it possible to load code to the device.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But the result is what you see in the last post in the memory browser.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Some flash is ok, but some regions have the problem with the error '?'&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;How can I 'repair' the fash?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR Lutz&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Mar 2021 12:14:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1251213#M10298</guid>
      <dc:creator>koehlerl</dc:creator>
      <dc:date>2021-03-24T12:14:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 no access via debug interface</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1252035#M10314</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can simply reprogram (by any example code) flash or erase it via debugger or via application.&lt;/P&gt;
&lt;P&gt;Have in mind to not leave empty boot vector at address 0x0 or the device will be locked.&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Thu, 25 Mar 2021 09:42:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1252035#M10314</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2021-03-25T09:42:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 no access via debug interface</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1252047#M10315</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;the problem ist, that the erase, reporgramming via debugger don't work correct.&lt;/P&gt;&lt;P&gt;Some memory regions have the problem with flash error. See meomery browser '?'.&lt;/P&gt;&lt;P&gt;So the application don't run. What must I do, that the flash is reprogrammed correct?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Lutz&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Mar 2021 09:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1252047#M10315</guid>
      <dc:creator>koehlerl</dc:creator>
      <dc:date>2021-03-25T09:54:09Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 no access via debug interface</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1254084#M10367</link>
      <description>&lt;P&gt;I need support to solve the problem !!!&lt;/P&gt;</description>
      <pubDate>Tue, 30 Mar 2021 07:32:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1254084#M10367</guid>
      <dc:creator>koehlerl</dc:creator>
      <dc:date>2021-03-30T07:32:31Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 no access via debug interface</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1254197#M10372</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;the problem ist, that the erase, reporgramming via debugger don't work correct.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Did you try it with PEMicro or Lauterbach? Or only via Segger? If you erase the memory from debugger, do you see success erase and the memory is still corrupt?&lt;/P&gt;
&lt;P&gt;Do you see the issue on all devices or on just one?&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;So the application don't run. What must I do, that the flash is reprogrammed correct?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;You need to erase/program memory correctly to have matching data with ECC syndrome in memory.&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Mar 2021 10:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-no-access-via-debug-interface/m-p/1254197#M10372</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2021-03-30T10:14:40Z</dc:date>
    </item>
  </channel>
</rss>