<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 T-BOX  S32K148</title>
    <link>https://community.nxp.com/t5/S32K/T-BOX-S32K148/m-p/1249147#M10248</link>
    <description>hi everybody! i have a problem, i can't connect MCU. try many times. I just have j-link. so how to solve this?? Connecting to J-Link... J-Link is connected. Firmware: J-Link V9 compiled May 17 2019 09:50:41 Checking target voltage... Target voltage: 3.33 V Listening on TCP/IP port 2331 Connecting to target...ERROR: InitTarget(): PCode returned with error code -1 ERROR: InitTarget(): PCode returned with error code -1 ERROR: Could not connect to target. Thanks. best wishes.</description>
    <pubDate>Sat, 20 Mar 2021 13:43:59 GMT</pubDate>
    <dc:creator>1971439734</dc:creator>
    <dc:date>2021-03-20T13:43:59Z</dc:date>
    <item>
      <title>T-BOX  S32K148</title>
      <link>https://community.nxp.com/t5/S32K/T-BOX-S32K148/m-p/1249147#M10248</link>
      <description>hi everybody! i have a problem, i can't connect MCU. try many times. I just have j-link. so how to solve this?? Connecting to J-Link... J-Link is connected. Firmware: J-Link V9 compiled May 17 2019 09:50:41 Checking target voltage... Target voltage: 3.33 V Listening on TCP/IP port 2331 Connecting to target...ERROR: InitTarget(): PCode returned with error code -1 ERROR: InitTarget(): PCode returned with error code -1 ERROR: Could not connect to target. Thanks. best wishes.</description>
      <pubDate>Sat, 20 Mar 2021 13:43:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/T-BOX-S32K148/m-p/1249147#M10248</guid>
      <dc:creator>1971439734</dc:creator>
      <dc:date>2021-03-20T13:43:59Z</dc:date>
    </item>
    <item>
      <title>Re: T-BOX  S32K148</title>
      <link>https://community.nxp.com/t5/S32K/T-BOX-S32K148/m-p/1249514#M10252</link>
      <description>&lt;P&gt;Please refer the method described in:&amp;nbsp;&lt;A href="https://mp.weixin.qq.com/s?__biz=MzI0MDk0ODcxMw==&amp;amp;mid=2247484245&amp;amp;idx=1&amp;amp;sn=3561b3bada7ab46acb3747ed9837769c&amp;amp;chksm=e91247d3de65cec51fb4b88556593da08b5e8613c2f487abbe593a7879cecdfbbe598b51ce11&amp;amp;scene=21#wechat_redirect" target="_self"&gt;S32K1xx系列MCU使用Tips--Flash加密后不断复位无法连接调试器的问题解决&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 09:06:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/T-BOX-S32K148/m-p/1249514#M10252</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-03-22T09:06:48Z</dc:date>
    </item>
  </channel>
</rss>