<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックs32k146evb CAN_PAL example issue</title>
    <link>https://community.nxp.com/t5/S32K/s32k146evb-CAN-PAL-example-issue/m-p/1248589#M10234</link>
    <description>&lt;P&gt;Got an offical s32k146 EVB board, created sample project from can_pal_s32k146 example, checked it from another commercial USBCAN box.&lt;/P&gt;&lt;P&gt;The USBCAN box complains sending error, which happened a lot with another board when the TJA1044 transceiver on that board was not enabled.&lt;/P&gt;&lt;P&gt;I am wondering if the UJA1169 transceiver on the official k146 EVB is not enabled by default?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 19 Mar 2021 04:38:19 GMT</pubDate>
    <dc:creator>yfliu</dc:creator>
    <dc:date>2021-03-19T04:38:19Z</dc:date>
    <item>
      <title>s32k146evb CAN_PAL example issue</title>
      <link>https://community.nxp.com/t5/S32K/s32k146evb-CAN-PAL-example-issue/m-p/1248589#M10234</link>
      <description>&lt;P&gt;Got an offical s32k146 EVB board, created sample project from can_pal_s32k146 example, checked it from another commercial USBCAN box.&lt;/P&gt;&lt;P&gt;The USBCAN box complains sending error, which happened a lot with another board when the TJA1044 transceiver on that board was not enabled.&lt;/P&gt;&lt;P&gt;I am wondering if the UJA1169 transceiver on the official k146 EVB is not enabled by default?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Mar 2021 04:38:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k146evb-CAN-PAL-example-issue/m-p/1248589#M10234</guid>
      <dc:creator>yfliu</dc:creator>
      <dc:date>2021-03-19T04:38:19Z</dc:date>
    </item>
    <item>
      <title>Re: s32k146evb CAN_PAL example issue</title>
      <link>https://community.nxp.com/t5/S32K/s32k146evb-CAN-PAL-example-issue/m-p/1248668#M10236</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi&amp;nbsp;yfliu,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;About how to use the SDK example, please refer the answer in&lt;/SPAN&gt;&lt;A href="https://community.nxp.com/t5/S32K/CAN-communication-on-s32k148EVB-Q144/m-p/1174290" target="_blank" rel="noopener" shape="rect"&gt;&amp;nbsp;CAN communication on s32k148EVB-Q144&lt;/A&gt;&lt;BR clear="none" /&gt;&lt;SPAN&gt;The setting may different between S32K146EVB and S32K148EVB, you need to check the example and documentation of S32K146EVB.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Notice external 12V power adapter is needed.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 19 Mar 2021 06:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k146evb-CAN-PAL-example-issue/m-p/1248668#M10236</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-03-19T06:43:56Z</dc:date>
    </item>
    <item>
      <title>Re: s32k146evb CAN_PAL example issue</title>
      <link>https://community.nxp.com/t5/S32K/s32k146evb-CAN-PAL-example-issue/m-p/1248717#M10242</link>
      <description>&lt;P&gt;Robin,&lt;/P&gt;&lt;P&gt;Used a 9V power adaptor for the K146EVB and now it works! Many thanks!&lt;/P&gt;&lt;P&gt;Previsouly I tried the example with another K144 customer board using just USB power, so wasn't aware of the importance of the power supply for CAN interface on K146EVB board.&lt;/P&gt;&lt;P&gt;yfliu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Mar 2021 08:13:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k146evb-CAN-PAL-example-issue/m-p/1248717#M10242</guid>
      <dc:creator>yfliu</dc:creator>
      <dc:date>2021-03-19T08:13:27Z</dc:date>
    </item>
  </channel>
</rss>