<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K144 FLEXCAN interrupt rx tx in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-FLEXCAN-interrupt-rx-tx/m-p/685057#M1022</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,Dear Support Team.&lt;/P&gt;&lt;P&gt;I now want to use S32K144 to an electronic project, but the relevant CAN DEMO example can refer to the small, I hope to be able to use CAN in the interrupt to receive, multiple ID data sent using the interrupt to send data, but the relevant S32DS Installation directory of the example, not much reference value, it is recommended S32K team can improve the relevant DEMO as soon as possible, so that application engineers can be applied as soon as possible in the actual project, shorten the development cycle, thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Jun 2017 08:43:21 GMT</pubDate>
    <dc:creator>wkei007</dc:creator>
    <dc:date>2017-06-13T08:43:21Z</dc:date>
    <item>
      <title>S32K144 FLEXCAN interrupt rx tx</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FLEXCAN-interrupt-rx-tx/m-p/685057#M1022</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,Dear Support Team.&lt;/P&gt;&lt;P&gt;I now want to use S32K144 to an electronic project, but the relevant CAN DEMO example can refer to the small, I hope to be able to use CAN in the interrupt to receive, multiple ID data sent using the interrupt to send data, but the relevant S32DS Installation directory of the example, not much reference value, it is recommended S32K team can improve the relevant DEMO as soon as possible, so that application engineers can be applied as soon as possible in the actual project, shorten the development cycle, thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 08:43:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FLEXCAN-interrupt-rx-tx/m-p/685057#M1022</guid>
      <dc:creator>wkei007</dc:creator>
      <dc:date>2017-06-13T08:43:21Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 FLEXCAN interrupt rx tx</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FLEXCAN-interrupt-rx-tx/m-p/685058#M1023</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/wkei007"&gt;wkei007&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case you have the Matlab/Simulink you can have a look here:&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-334170"&gt;https://community.nxp.com/docs/DOC-334170&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is one sample:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20535iEB904452316E6BE9/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.JPG" alt="1.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since everything is Simulink based with Automatic code generation - the prototyping is faster.&lt;/P&gt;&lt;P&gt;We have many other examples as well but what is interesting in model based design approach is the simplicity to enhance the default models to do what ever you wish for. Here is the whole collection:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Capture.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20536i06E4FB486498FB3A/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.JPG" alt="Capture.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 09:57:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FLEXCAN-interrupt-rx-tx/m-p/685058#M1023</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2017-06-13T09:57:13Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 FLEXCAN interrupt rx tx</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FLEXCAN-interrupt-rx-tx/m-p/685059#M1024</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Oh, that in order to apply this FLEX_CAN interrupt send and receive, I have to learn about the use of Matlab / Simulink, thank you&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 23:55:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FLEXCAN-interrupt-rx-tx/m-p/685059#M1024</guid>
      <dc:creator>wkei007</dc:creator>
      <dc:date>2017-06-13T23:55:30Z</dc:date>
    </item>
  </channel>
</rss>