<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Using FTM input capture for capturing ultrasonic data</title>
    <link>https://community.nxp.com/t5/S32K/Using-FTM-input-capture-for-capturing-ultrasonic-data/m-p/1243272#M10113</link>
    <description>&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;We aren't using UART to capture the signal from the USS. Instead we have connected the USS_RX pin directly to the PTD15 pin which is configured to FTM0_CH0. We have used the FTM input capture component from the s32 SDK. Can you please provide the code/example for the same??&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Shravan Manerikar&lt;/P&gt;</description>
    <pubDate>Wed, 10 Mar 2021 12:51:54 GMT</pubDate>
    <dc:creator>shravanmanerikar</dc:creator>
    <dc:date>2021-03-10T12:51:54Z</dc:date>
    <item>
      <title>Using FTM input capture for capturing ultrasonic data</title>
      <link>https://community.nxp.com/t5/S32K/Using-FTM-input-capture-for-capturing-ultrasonic-data/m-p/1242508#M10098</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a custom board having an s32k146. I am using FreeRTOS for running the s32k. I want to use the FTM input capture mode to detect the data sent using an ultrasonic sensor, which is using pulse coded protocol for data communication with the s32k. My PTD16 pin is configured as GPIO which is configured for output mode i.e it sends command from the s32k to the USS. PTD15 is configured as FTM in input mode i.e it will receive the data sent from the USS.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I do not know how to use the FTM input capture mode to detect the signal. Currently I have configured the FTM as follows:&lt;/P&gt;&lt;P&gt;//flexTimer_ic1.c&lt;/P&gt;&lt;P&gt;ftm_input_ch_param_t flexTimer_ic1_InputCaptureChannelConfig[1] =&lt;BR /&gt;{&lt;BR /&gt;{&lt;BR /&gt;0U, /* Channel id */&lt;BR /&gt;FTM_SIGNAL_MEASUREMENT, /* Input capture operation mode */&lt;BR /&gt;FTM_RISING_EDGE, /* Edge alignment mode */&lt;BR /&gt;FTM_PERIOD_OFF_MEASUREMENT, /* Signal measurement operation type */&lt;BR /&gt;0U, /* Filter value */&lt;BR /&gt;false, /* Filter state (enabled/disabled) */&lt;BR /&gt;true, /* Continuous measurement state */&lt;BR /&gt;NULL, /* Vector of callbacks parameters for channels events */&lt;BR /&gt;NULL /* Vector of callbacks for channels events */&lt;BR /&gt;}&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;and this is how I initialize it&lt;/P&gt;&lt;P&gt;//main.c&lt;/P&gt;&lt;P&gt;/* Initialize FTM instances, PWM and Input capture&lt;BR /&gt;* - See ftm component for more details&lt;BR /&gt;*/&lt;BR /&gt;FTM_DRV_Init(INST_FLEXTIMER_IC1, &amp;amp;flexTimer_ic1_InitConfig, &amp;amp;ftm1StateStruct);&lt;/P&gt;&lt;P&gt;/* Setup input capture for FTM 1 channel 0 - PTB2 */&lt;BR /&gt;FTM_DRV_InitInputCapture(INST_FLEXTIMER_IC1, &amp;amp;flexTimer_ic1_InputCaptureConfig);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Kindly help me understand write the logic to use this FTM component to read the data from the data line&lt;/P&gt;&lt;P&gt;I am attaching a screenshot of the data which is sent by the USS.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Mar 2021 11:51:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-FTM-input-capture-for-capturing-ultrasonic-data/m-p/1242508#M10098</guid>
      <dc:creator>shravanmanerikar</dc:creator>
      <dc:date>2021-03-09T11:51:38Z</dc:date>
    </item>
    <item>
      <title>Re: Using FTM input capture for capturing ultrasonic data</title>
      <link>https://community.nxp.com/t5/S32K/Using-FTM-input-capture-for-capturing-ultrasonic-data/m-p/1243014#M10107</link>
      <description>&lt;P&gt;Hi&amp;nbsp;shravanmanerikar,&lt;/P&gt;
&lt;P&gt;If pulse coded protocol means: Single Edge Nibble Transmission protocol (SENT, SAE J2716)&lt;/P&gt;
&lt;P&gt;Then there are two examples that you can refer:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/SENT-receiver-for-S32K118-Design-Studio/ta-p/1127356" target="_self"&gt;SENT receiver for S32K118 Design Studio&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Uart-to-SENT-protocol-transmitter/ta-p/1129291" target="_self"&gt;Uart to SENT protocol transmitter&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 07:16:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-FTM-input-capture-for-capturing-ultrasonic-data/m-p/1243014#M10107</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-03-10T07:16:45Z</dc:date>
    </item>
    <item>
      <title>Re: Using FTM input capture for capturing ultrasonic data</title>
      <link>https://community.nxp.com/t5/S32K/Using-FTM-input-capture-for-capturing-ultrasonic-data/m-p/1243272#M10113</link>
      <description>&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;We aren't using UART to capture the signal from the USS. Instead we have connected the USS_RX pin directly to the PTD15 pin which is configured to FTM0_CH0. We have used the FTM input capture component from the s32 SDK. Can you please provide the code/example for the same??&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Shravan Manerikar&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 12:51:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-FTM-input-capture-for-capturing-ultrasonic-data/m-p/1243272#M10113</guid>
      <dc:creator>shravanmanerikar</dc:creator>
      <dc:date>2021-03-10T12:51:54Z</dc:date>
    </item>
    <item>
      <title>Re: Using FTM input capture for capturing ultrasonic data</title>
      <link>https://community.nxp.com/t5/S32K/Using-FTM-input-capture-for-capturing-ultrasonic-data/m-p/1244079#M10131</link>
      <description>&lt;P&gt;We do not have a project that fully meets your requirements. You can refer the project attached in &lt;A href="https://community.nxp.com/t5/S32K/How-to-use-FlexIO-configuration-to-SENT-SAE-J2716/m-p/850812" target="_self"&gt;How to use FlexIO configuration to SENT(SAE-J2716).&lt;/A&gt; &lt;SPAN&gt; The &lt;A href="https://www.nxp.com/docs/en/data-sheet/KMA320.pdf" target="_self"&gt;KMA320&lt;/A&gt; is configured to transmit the angle values via SENT interface, and S32K144 captures each pulse in the SENT frame by FlexTimer input-capture feature, then triggers DMA request.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Mar 2021 09:34:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-FTM-input-capture-for-capturing-ultrasonic-data/m-p/1244079#M10131</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-03-11T09:34:52Z</dc:date>
    </item>
  </channel>
</rss>