<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K144 IIC</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-IIC/m-p/1243226#M10112</link>
    <description>&lt;P&gt;hello,dear&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a problem and need your help.&lt;BR /&gt;When I use the IIC module, it is set to master mode, and the slave address is set to 0X1A through configuration, but the address is found to be 0x34 through the logic analyzer. Moved one place to the left. How can I solve this?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SimonWangyu_0-1615375008419.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/139252i30C276C8A2159B16/image-size/medium?v=v2&amp;amp;px=400" role="button" title="SimonWangyu_0-1615375008419.png" alt="SimonWangyu_0-1615375008419.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SimonWangyu_1-1615375047287.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/139253iFC9C720C7CB8F427/image-size/medium?v=v2&amp;amp;px=400" role="button" title="SimonWangyu_1-1615375047287.png" alt="SimonWangyu_1-1615375047287.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 10 Mar 2021 11:22:58 GMT</pubDate>
    <dc:creator>SimonWangyu</dc:creator>
    <dc:date>2021-03-10T11:22:58Z</dc:date>
    <item>
      <title>S32K144 IIC</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-IIC/m-p/1243226#M10112</link>
      <description>&lt;P&gt;hello,dear&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a problem and need your help.&lt;BR /&gt;When I use the IIC module, it is set to master mode, and the slave address is set to 0X1A through configuration, but the address is found to be 0x34 through the logic analyzer. Moved one place to the left. How can I solve this?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SimonWangyu_0-1615375008419.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/139252i30C276C8A2159B16/image-size/medium?v=v2&amp;amp;px=400" role="button" title="SimonWangyu_0-1615375008419.png" alt="SimonWangyu_0-1615375008419.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SimonWangyu_1-1615375047287.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/139253iFC9C720C7CB8F427/image-size/medium?v=v2&amp;amp;px=400" role="button" title="SimonWangyu_1-1615375047287.png" alt="SimonWangyu_1-1615375047287.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 11:22:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-IIC/m-p/1243226#M10112</guid>
      <dc:creator>SimonWangyu</dc:creator>
      <dc:date>2021-03-10T11:22:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 IIC</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-IIC/m-p/1243293#M10114</link>
      <description>&lt;P&gt;Hello Simon,&lt;/P&gt;
&lt;P&gt;The address consists of the Slave address (0x1A) at address[7:1] + the W/R bit at address[0].&lt;/P&gt;
&lt;P&gt;Write address 0x34 = 0b0011_0100&lt;/P&gt;
&lt;P&gt;Read address 0x35 = 0b0011_0101&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 13:17:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-IIC/m-p/1243293#M10114</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-03-10T13:17:18Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 IIC</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-IIC/m-p/1243716#M10125</link>
      <description>&lt;P&gt;Very happy to receive a reply. I want to add that the slave address that needs to communicate is 0x1A. And there are other devices that can communicate normally, and the slave address I collected through the logic analyzer is also 0X1A. But when I switch to S32K144, the configuration is also 0X1A, but the address collected by the logic analyzer is 0x34. Why is this? And because the address is wrong, the slave does not respond to the command.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Mar 2021 00:41:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-IIC/m-p/1243716#M10125</guid>
      <dc:creator>SimonWangyu</dc:creator>
      <dc:date>2021-03-11T00:41:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 IIC</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-IIC/m-p/1244010#M10129</link>
      <description>&lt;P&gt;Hi Simon,&lt;/P&gt;
&lt;P&gt;As I said already, the configuration tool sets the address[7:1] bits.&lt;/P&gt;
&lt;P&gt;Use 0x0D instead.&lt;/P&gt;
&lt;P&gt;address[7:0] = 0x1A = 0b00011010 where address[4:1] is 0xD.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 11 Mar 2021 08:34:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-IIC/m-p/1244010#M10129</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-03-11T08:34:14Z</dc:date>
    </item>
  </channel>
</rss>