<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32k14x debugging with external device in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32k14x-debugging-with-external-device/m-p/1242329#M10094</link>
    <description>&lt;P&gt;Hi, thank you for your reply. I thought this will work as normal openSDA debugger, in which i will put firmware (same as for K20 on eval board) and will work, but unfortunatelly it's not - compared to K20 on eval-board it has only 64 kb bootloader memory, and k20 has 128 MB! I tried to drag-and-drop hex file through that programmer, but it outputs fail :&lt;BR /&gt;The interface firmware FAILED to download the flash programming algorithms to the target MCU&lt;/P&gt;</description>
    <pubDate>Tue, 09 Mar 2021 08:04:05 GMT</pubDate>
    <dc:creator>maksym_leski</dc:creator>
    <dc:date>2021-03-09T08:04:05Z</dc:date>
    <item>
      <title>S32k14x debugging with external device</title>
      <link>https://community.nxp.com/t5/S32K/S32k14x-debugging-with-external-device/m-p/1241769#M10083</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I am developing device using S32K142 and I have bought cheap programmer ZL33PRG&lt;BR /&gt;&lt;A href="https://www.tme.eu/pl/details/zl33prg/programatory/" target="_blank"&gt;https://www.tme.eu/pl/details/zl33prg/programatory/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It should be compatilible with OpenSDA that is on S32K144-EVB, but when I try to load firmware from PEmicro it says the .sda file is too big (over 64kb). Is there any way to make it work? Or should I buy something else? I know I can use EVB for debugging purposes but this isn't comfortable.&lt;/P&gt;&lt;P&gt;Ofc the S32DS isn't detecting this ZL33PRG&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Max&lt;/P&gt;</description>
      <pubDate>Mon, 08 Mar 2021 13:04:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k14x-debugging-with-external-device/m-p/1241769#M10083</guid>
      <dc:creator>maksym_leski</dc:creator>
      <dc:date>2021-03-08T13:04:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32k14x debugging with external device</title>
      <link>https://community.nxp.com/t5/S32K/S32k14x-debugging-with-external-device/m-p/1241861#M10088</link>
      <description>&lt;P&gt;Hi, I would recommend to contact a programmer's manufacturer. I am afraid we cannot help with third party tool we don't have experience with.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Mar 2021 16:28:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k14x-debugging-with-external-device/m-p/1241861#M10088</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-03-08T16:28:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32k14x debugging with external device</title>
      <link>https://community.nxp.com/t5/S32K/S32k14x-debugging-with-external-device/m-p/1242329#M10094</link>
      <description>&lt;P&gt;Hi, thank you for your reply. I thought this will work as normal openSDA debugger, in which i will put firmware (same as for K20 on eval board) and will work, but unfortunatelly it's not - compared to K20 on eval-board it has only 64 kb bootloader memory, and k20 has 128 MB! I tried to drag-and-drop hex file through that programmer, but it outputs fail :&lt;BR /&gt;The interface firmware FAILED to download the flash programming algorithms to the target MCU&lt;/P&gt;</description>
      <pubDate>Tue, 09 Mar 2021 08:04:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k14x-debugging-with-external-device/m-p/1242329#M10094</guid>
      <dc:creator>maksym_leski</dc:creator>
      <dc:date>2021-03-09T08:04:05Z</dc:date>
    </item>
  </channel>
</rss>