<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K144 code execution doesn't start after power cycle</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-code-execution-doesn-t-start-after-power-cycle/m-p/1241696#M10080</link>
    <description>&lt;P&gt;Hello everyone.&lt;/P&gt;&lt;P&gt;Hope you're safe and sound.&lt;/P&gt;&lt;P&gt;My problem: after the code has been build and loaded on the target it works, but when I do a power cycle (power off, then on) the code doesn't start at all.&lt;/P&gt;&lt;P&gt;I did my development on a S32K142Q100 EVB and everything was fine.&lt;/P&gt;&lt;P&gt;Then I moved to my target PCBA which is with S32K144 (FS32K144ULT0VLLT). I think I've done all my settings correctly, considering the migration to the S32K144, incl. proper project settings (S32DS 2018.R1), replacing linker file (btw I use S32K144_64_flash.ld from the SDK).&lt;/P&gt;&lt;P&gt;My debugger is P&amp;amp;E micro Multilink universal, but I also tried it with Lauterbach's Trace32.&lt;/P&gt;&lt;P&gt;Can you suggest what miserable setting in the S32DS have I put wrong ...&lt;/P&gt;&lt;P&gt;I'll appreciate any help, and thanks for your time.&lt;/P&gt;</description>
    <pubDate>Mon, 08 Mar 2021 10:33:38 GMT</pubDate>
    <dc:creator>munchosmith</dc:creator>
    <dc:date>2021-03-08T10:33:38Z</dc:date>
    <item>
      <title>S32K144 code execution doesn't start after power cycle</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-code-execution-doesn-t-start-after-power-cycle/m-p/1241696#M10080</link>
      <description>&lt;P&gt;Hello everyone.&lt;/P&gt;&lt;P&gt;Hope you're safe and sound.&lt;/P&gt;&lt;P&gt;My problem: after the code has been build and loaded on the target it works, but when I do a power cycle (power off, then on) the code doesn't start at all.&lt;/P&gt;&lt;P&gt;I did my development on a S32K142Q100 EVB and everything was fine.&lt;/P&gt;&lt;P&gt;Then I moved to my target PCBA which is with S32K144 (FS32K144ULT0VLLT). I think I've done all my settings correctly, considering the migration to the S32K144, incl. proper project settings (S32DS 2018.R1), replacing linker file (btw I use S32K144_64_flash.ld from the SDK).&lt;/P&gt;&lt;P&gt;My debugger is P&amp;amp;E micro Multilink universal, but I also tried it with Lauterbach's Trace32.&lt;/P&gt;&lt;P&gt;Can you suggest what miserable setting in the S32DS have I put wrong ...&lt;/P&gt;&lt;P&gt;I'll appreciate any help, and thanks for your time.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Mar 2021 10:33:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-code-execution-doesn-t-start-after-power-cycle/m-p/1241696#M10080</guid>
      <dc:creator>munchosmith</dc:creator>
      <dc:date>2021-03-08T10:33:38Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 code execution doesn't start after power cycle</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-code-execution-doesn-t-start-after-power-cycle/m-p/1241812#M10086</link>
      <description>&lt;P&gt;It appears that with one additional reset the code eventually starts executing...&lt;/P&gt;</description>
      <pubDate>Mon, 08 Mar 2021 14:57:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-code-execution-doesn-t-start-after-power-cycle/m-p/1241812#M10086</guid>
      <dc:creator>munchosmith</dc:creator>
      <dc:date>2021-03-08T14:57:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 code execution doesn't start after power cycle</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-code-execution-doesn-t-start-after-power-cycle/m-p/1242483#M10096</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/153949"&gt;@munchosmith&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The MCU must always do something.&lt;/P&gt;
&lt;P&gt;If it does not keep resetting itself, the application is stuck somewhere.&lt;/P&gt;
&lt;P&gt;You can attach the Multilink and examine the state of the MCU.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1615288776825.png" style="width: 504px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/139124i06B3ECABF5DB2419/image-dimensions/504x388?v=v2" width="504" height="388" role="button" title="danielmartynek_0-1615288776825.png" alt="danielmartynek_0-1615288776825.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 09 Mar 2021 11:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-code-execution-doesn-t-start-after-power-cycle/m-p/1242483#M10096</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-03-09T11:21:02Z</dc:date>
    </item>
  </channel>
</rss>