<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Issue with LPUART</title>
    <link>https://community.nxp.com/t5/S32K/Issue-with-LPUART/m-p/1240188#M10058</link>
    <description>&lt;P&gt;1.lpuart echo s32k116&lt;/P&gt;&lt;P&gt;2.custom board&lt;/P&gt;&lt;P&gt;3.rx-PTC2&amp;nbsp; &amp;nbsp;tx-PTC3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 04 Mar 2021 10:04:55 GMT</pubDate>
    <dc:creator>pankajprasad100</dc:creator>
    <dc:date>2021-03-04T10:04:55Z</dc:date>
    <item>
      <title>Issue with LPUART</title>
      <link>https://community.nxp.com/t5/S32K/Issue-with-LPUART/m-p/1239383#M10048</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I am working with S32K116 in which using example code for LPUART.&lt;/P&gt;&lt;P&gt;While checking the signals using oscilloscope i can see highs and lows but the voltage levels are in 250 to 300 mV range.&lt;/P&gt;&lt;P&gt;Well i think voltage levels should be should be in volts not in milli volts.&lt;/P&gt;&lt;P&gt;Any reason behind it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;PANKAJ PRASAD&lt;/P&gt;</description>
      <pubDate>Wed, 03 Mar 2021 13:07:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-with-LPUART/m-p/1239383#M10048</guid>
      <dc:creator>pankajprasad100</dc:creator>
      <dc:date>2021-03-03T13:07:01Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LPUART</title>
      <link>https://community.nxp.com/t5/S32K/Issue-with-LPUART/m-p/1239439#M10051</link>
      <description>&lt;P&gt;Hi Pankaj,&lt;/P&gt;
&lt;P&gt;Which LPUART examples do you use?&lt;/P&gt;
&lt;P&gt;Do you have an EVB or your custom board?&lt;/P&gt;
&lt;P&gt;Which pins do you scope?&lt;/P&gt;
&lt;P&gt;The voltage levels depends on the power supply as you can see in the DS, rev.13, Chapter 5, I/O parameters.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 03 Mar 2021 14:33:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-with-LPUART/m-p/1239439#M10051</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-03-03T14:33:21Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LPUART</title>
      <link>https://community.nxp.com/t5/S32K/Issue-with-LPUART/m-p/1240188#M10058</link>
      <description>&lt;P&gt;1.lpuart echo s32k116&lt;/P&gt;&lt;P&gt;2.custom board&lt;/P&gt;&lt;P&gt;3.rx-PTC2&amp;nbsp; &amp;nbsp;tx-PTC3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Mar 2021 10:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-with-LPUART/m-p/1240188#M10058</guid>
      <dc:creator>pankajprasad100</dc:creator>
      <dc:date>2021-03-04T10:04:55Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LPUART</title>
      <link>https://community.nxp.com/t5/S32K/Issue-with-LPUART/m-p/1241811#M10085</link>
      <description>&lt;P&gt;Hello Pankaj,&lt;/P&gt;
&lt;P&gt;The issue was reportedly solved.&lt;/P&gt;
&lt;P&gt;If not, let me know.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Mar 2021 14:57:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-with-LPUART/m-p/1241811#M10085</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-03-08T14:57:01Z</dc:date>
    </item>
  </channel>
</rss>