<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックVR5510 reset when use lauterbach debug</title>
    <link>https://community.nxp.com/t5/S32G/VR5510-reset-when-use-lauterbach-debug/m-p/1484474#M994</link>
    <description>&lt;P&gt;hi, NXP,&amp;nbsp;&lt;/P&gt;&lt;P&gt;When using Lauterbach to debug the initialization program with the PMIC vr5510, once the cpu reset is used, the PMIC will be powered on and off again, because the PMIC detects that there is a reset signal in RESET_B in&amp;#8; MCU.&lt;BR /&gt;My question is, how to turn off RSTB detection during PMIC initialization so that PMIC will not restart when debugging with Lauterbach.&lt;/P&gt;</description>
    <pubDate>Tue, 05 Jul 2022 08:00:27 GMT</pubDate>
    <dc:creator>nioer</dc:creator>
    <dc:date>2022-07-05T08:00:27Z</dc:date>
    <item>
      <title>VR5510 reset when use lauterbach debug</title>
      <link>https://community.nxp.com/t5/S32G/VR5510-reset-when-use-lauterbach-debug/m-p/1484474#M994</link>
      <description>&lt;P&gt;hi, NXP,&amp;nbsp;&lt;/P&gt;&lt;P&gt;When using Lauterbach to debug the initialization program with the PMIC vr5510, once the cpu reset is used, the PMIC will be powered on and off again, because the PMIC detects that there is a reset signal in RESET_B in&amp;#8; MCU.&lt;BR /&gt;My question is, how to turn off RSTB detection during PMIC initialization so that PMIC will not restart when debugging with Lauterbach.&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jul 2022 08:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/VR5510-reset-when-use-lauterbach-debug/m-p/1484474#M994</guid>
      <dc:creator>nioer</dc:creator>
      <dc:date>2022-07-05T08:00:27Z</dc:date>
    </item>
  </channel>
</rss>